<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: BeeKit Test Tool Fails to recognize the virtual comport (device) in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeKit-Test-Tool-Fails-to-recognize-the-virtual-comport-device/m-p/160288#M9632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try to run the Test Tool as Administrator and It will works with others virtual COM. &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Nov 2011 16:32:29 GMT</pubDate>
    <dc:creator>Xarxas</dc:creator>
    <dc:date>2011-11-03T16:32:29Z</dc:date>
    <item>
      <title>BeeKit Test Tool Fails to recognize the virtual comport (device)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeKit-Test-Tool-Fails-to-recognize-the-virtual-comport-device/m-p/160287#M9631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello~~&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I &amp;nbsp;installed Beekit 1.9.17 onto a &amp;nbsp;Windows 7.&lt;/P&gt;&lt;P&gt;When I launch Test tool from Beekit. The communication settings found no comport of my device (see attached picture). However, my device is shown in the Device manager window. My device is a SBR board &amp;nbsp;with CP2102 as the virtual comport interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can use the same board to communicate with Hyperterminal or other serial program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder whether this is because of the CP2102's driver version. I am using the Silab driver included with Beekit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But Test tool failed to found my device as described above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use the same board on another PC (with older version of CP2102). Everything work fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help....&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Nov 2010 07:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeKit-Test-Tool-Fails-to-recognize-the-virtual-comport-device/m-p/160287#M9631</guid>
      <dc:creator>greatbigman</dc:creator>
      <dc:date>2010-11-04T07:24:13Z</dc:date>
    </item>
    <item>
      <title>Re: BeeKit Test Tool Fails to recognize the virtual comport (device)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeKit-Test-Tool-Fails-to-recognize-the-virtual-comport-device/m-p/160288#M9632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try to run the Test Tool as Administrator and It will works with others virtual COM. &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2011 16:32:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeKit-Test-Tool-Fails-to-recognize-the-virtual-comport-device/m-p/160288#M9632</guid>
      <dc:creator>Xarxas</dc:creator>
      <dc:date>2011-11-03T16:32:29Z</dc:date>
    </item>
  </channel>
</rss>