<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Virtual com port with JB16 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126167#M961</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;has someone tried to implemant a virtual com ort with a 68hc908jb16 to use it as a rs232 to usb converter ? What has to be done on the windows side to get this working ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Eckhard&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Feb 2006 04:16:41 GMT</pubDate>
    <dc:creator>eckhard</dc:creator>
    <dc:date>2006-02-10T04:16:41Z</dc:date>
    <item>
      <title>Virtual com port with JB16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126167#M961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;has someone tried to implemant a virtual com ort with a 68hc908jb16 to use it as a rs232 to usb converter ? What has to be done on the windows side to get this working ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Eckhard&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2006 04:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126167#M961</guid>
      <dc:creator>eckhard</dc:creator>
      <dc:date>2006-02-10T04:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual com port with JB16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126168#M962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I looked into this for a USB project, but determined that it would not work well.&lt;BR /&gt;&lt;BR /&gt;The reason is that the JB16 does not support full-speed (12 mbps), it only supports low-speed (1.5 mbps). Though this sounds fast enough, the USB spec puts restrictions on low-speed operation:&lt;BR /&gt;&lt;BR /&gt;1) You can only use control messages and interrupt messages. Isochronous messages (what USB-to-Serial adapters usually use) are not available to low-speed devices.&lt;BR /&gt;&lt;BR /&gt;2) A low-speed device cannot issue interrupt messages more often than every 10 millisecond. Also, the payload for those messages cannot be more than eight bytes.&lt;BR /&gt;&lt;BR /&gt;This meant that I could not push more than 800 bytes per second across the USB. That equated to a maximum baud rate of 8 Kbaud, way too slow for my needs.&lt;BR /&gt;&lt;BR /&gt;I ended up using an FDDI chip (a very simple solution) hooked up to a HC08GP32. The FDDI chip is fully supported at the host side, and simply shows up as another COMM port.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2006 06:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126168#M962</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-02-10T06:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual com port with JB16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126169#M963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;maybe thats why i haven´t found anything about that. Hard to believe that the JB16 cannot handle this and the FTDi chip can do it so easy.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eckhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2006 17:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126169#M963</guid>
      <dc:creator>eckhard</dc:creator>
      <dc:date>2006-02-10T17:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual com port with JB16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126170#M964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;eckhard wrote:&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;. . . and the FTDi chip can do it so easy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Eckhard&lt;/P&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;Then again, that is all that the FTDI chip does, so it does it well.&lt;BR /&gt;&lt;BR /&gt;Freescale uses FTDI's FT232BM chip on one of their ZigBee boards (DIG528), connected to the MC9S08GT60. They have the schematic on the website (somewhere, Document Number 80000528000_R0203.DSN) if you need a reference design.&lt;P&gt;Message Edited by rocco on &lt;SPAN class="date_text"&gt;02-10-2006&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:30 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Feb 2006 03:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126170#M964</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-02-11T03:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual com port with JB16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126171#M965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I look at cypress. it have the "Virtual com port" .use low speed usb mcu and HID class. who can move it to hc08?&lt;/DIV&gt;&lt;DIV&gt;It's speed:600-56K baud (800 bytes/sec)&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.cypress.com/portal/server.pt?space=CommunityPage&amp;amp;control=SetCommunity&amp;amp;CommunityID=209&amp;amp;PageID=418&amp;amp;r_folder=Reference%20Designs&amp;amp;r_title=CY4601%20USB%20to%20Serial" rel="nofollow" target="_blank"&gt;http://www.cypress.com/portal/server.pt?space=CommunityPage&amp;amp;control=SetCommunity&amp;amp;CommunityID=209&amp;amp;PageID=418&amp;amp;r_folder=Reference%20Designs&amp;amp;r_title=CY4601%20USB%20to%20Serial&lt;/A&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2006 10:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Virtual-com-port-with-JB16/m-p/126171#M965</guid>
      <dc:creator>l456789</dc:creator>
      <dc:date>2006-03-08T10:56:23Z</dc:date>
    </item>
  </channel>
</rss>