<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JM60 USB bootloader driver download in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159176#M9432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a problem with the JM60 USB bootloader driver. When I connect the EfmJM60 autoprogrammable module to a pc with windows XP, it works correctly, but when I work in a pc with windows 7, the pc detects the device with a name different to JM60 but the JMGui doesn't detect it. Should I install a special driver for windows 7? What must I do? I need your help. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Oct 2014 14:33:34 GMT</pubDate>
    <dc:creator>cesar_osorio</dc:creator>
    <dc:date>2014-10-28T14:33:34Z</dc:date>
    <item>
      <title>JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159173#M9429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does anyone know where I can download the JM60 USB driver for Windows XP and Windows Embedded Standard 7?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2011 14:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159173#M9429</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-08-12T14:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159174#M9430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The app note, &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3582.pdf" rel="nofollow" target="_self"&gt;AN3582 : The USB Data Logger based on the MC9S08JM60&lt;/A&gt;﻿, describes a data logging application on a PC that uses the USB interface. The software for the app note is in the archive, AN3582SW.zip. This should help you get started.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2011 19:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159174#M9430</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-08-15T19:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159175#M9431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear J2MEJediMaster,&lt;/P&gt;&lt;P&gt;I mean the &lt;EM&gt;&lt;STRONG&gt;bootloader&lt;/STRONG&gt;&lt;/EM&gt; driver (Windows 7 - 64bit) for JM60.&lt;/P&gt;&lt;P&gt;I have JM60_GUI - which has the PC driver package including the WdfCoInstallerxxxxx.dll, WinUSBCoInstaller.dll and *.inf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I am not sure if these files can be used for Windows 7 64bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please kindly advise. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2011 08:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159175#M9431</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-08-16T08:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159176#M9432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a problem with the JM60 USB bootloader driver. When I connect the EfmJM60 autoprogrammable module to a pc with windows XP, it works correctly, but when I work in a pc with windows 7, the pc detects the device with a name different to JM60 but the JMGui doesn't detect it. Should I install a special driver for windows 7? What must I do? I need your help. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 14:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159176#M9432</guid>
      <dc:creator>cesar_osorio</dc:creator>
      <dc:date>2014-10-28T14:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159177#M9433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cesar,&lt;/P&gt;&lt;P&gt;You need new driver for 64-bit. Below is the reply I got from FSL Technical Support:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The installer version that I have sent you includes a&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;newer version of WinUSB driver, allowing compatibility with 64-bit Windows&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;versions. We have tested this version on Windows XP, Vista and Seven, on 32 and&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;64 bits and worked as expected, while the version available on the website is&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;compatible with 32-bit only. We are in process of upload the updated version on&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;the website.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hope this will be useful for you. Please let me know if&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;you have further questions. Have a nice day.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Should you need to contact us with regard to this&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;message, please see the notes below. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Best Regards,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Carlos Jose&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Technical Information &amp;amp; Commercial Support &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Freescale Semiconductor"&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 01:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159177#M9433</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2014-10-29T01:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: Re: JM60 USB bootloader driver download</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159178#M9434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Augusto:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As SP Lee mentioned, you need a newer version of JM60 Bootloader GUI. Attached is what I think is the latest version available, and should be compatible with Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyalert: You have to uninstall previous versions of the GUI before running the installer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 03:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-USB-bootloader-driver-download/m-p/159178#M9434</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-29T03:44:32Z</dc:date>
    </item>
  </channel>
</rss>