<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCU in MC13213 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-in-MC13213/m-p/159147#M9428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and welcome to the forums Thomas,&lt;BR /&gt;&lt;BR /&gt;The chip inside a GB60 and a GT60 is exactly the same.&lt;BR /&gt;The are all mask xL31R (x = 1 to 4)&lt;BR /&gt;The GT simply has less pads bonded out to pins.&lt;BR /&gt;The MC13213 does not have all pins bonded out either and so is closer to a GT.&lt;BR /&gt;You can still use the higher timer channels and such, you just don't have the channel pins etc.&lt;BR /&gt;&lt;BR /&gt;With the A versions of the GT they have actually cut down the die to more closely tie in with what is actually bonded out.&lt;BR /&gt;But I believe the Zigbee stuff still uses the old GB/GT (non-A)&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 May 2008 18:23:14 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2008-05-27T18:23:14Z</dc:date>
    <item>
      <title>MCU in MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-in-MC13213/m-p/159146#M9427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please could anyone tell me which controller is in the MC13213 RF transceiver? It should be an MC9S08GB60 or a MC9SGT60.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thomas&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2008 15:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-in-MC13213/m-p/159146#M9427</guid>
      <dc:creator>Thomas_H</dc:creator>
      <dc:date>2008-05-27T15:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCU in MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-in-MC13213/m-p/159147#M9428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and welcome to the forums Thomas,&lt;BR /&gt;&lt;BR /&gt;The chip inside a GB60 and a GT60 is exactly the same.&lt;BR /&gt;The are all mask xL31R (x = 1 to 4)&lt;BR /&gt;The GT simply has less pads bonded out to pins.&lt;BR /&gt;The MC13213 does not have all pins bonded out either and so is closer to a GT.&lt;BR /&gt;You can still use the higher timer channels and such, you just don't have the channel pins etc.&lt;BR /&gt;&lt;BR /&gt;With the A versions of the GT they have actually cut down the die to more closely tie in with what is actually bonded out.&lt;BR /&gt;But I believe the Zigbee stuff still uses the old GB/GT (non-A)&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2008 18:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-in-MC13213/m-p/159147#M9428</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-05-27T18:23:14Z</dc:date>
    </item>
  </channel>
</rss>