<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: qg8 sci at 115200 baud?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126146#M942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;A very related question to the question above.&lt;BR /&gt;&lt;BR /&gt;Is it possible to configure QE128 (guess it has the same ICS as qg8) to 230400 baud with ICS? Im having a hard time figuring out all the dividers and ICRs etc. for that to be possible...&lt;BR /&gt;&lt;BR /&gt;Best regards Henrik&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2008 22:09:12 GMT</pubDate>
    <dc:creator>hek</dc:creator>
    <dc:date>2008-02-12T22:09:12Z</dc:date>
    <item>
      <title>qg8 sci at 115200 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126143#M939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is it possible to configure the SCI in the&amp;nbsp;9S08QG8 to run at 115200 baud using the internal clock?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2006 21:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126143#M939</guid>
      <dc:creator>jim</dc:creator>
      <dc:date>2006-08-09T21:35:01Z</dc:date>
    </item>
    <item>
      <title>Re: qg8 sci at 115200 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126144#M940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Sure is. There's a QG8 right behind me sending/receiving data at that rate right now.&lt;BR /&gt;&lt;BR /&gt;You have to calibrate the ICS for 36KHz to get a BUSCLK of 9.216MHz, then set the SCI baud rate register to 5.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2006 00:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126144#M940</guid>
      <dc:creator>Wings</dc:creator>
      <dc:date>2006-08-10T00:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: qg8 sci at 115200 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126145#M941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2006 01:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126145#M941</guid>
      <dc:creator>jim</dc:creator>
      <dc:date>2006-08-10T01:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: qg8 sci at 115200 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126146#M942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;A very related question to the question above.&lt;BR /&gt;&lt;BR /&gt;Is it possible to configure QE128 (guess it has the same ICS as qg8) to 230400 baud with ICS? Im having a hard time figuring out all the dividers and ICRs etc. for that to be possible...&lt;BR /&gt;&lt;BR /&gt;Best regards Henrik&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2008 22:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/qg8-sci-at-115200-baud/m-p/126146#M942</guid>
      <dc:creator>hek</dc:creator>
      <dc:date>2008-02-12T22:09:12Z</dc:date>
    </item>
  </channel>
</rss>