<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックProblem by resetting the HC08GZ32 with MON08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158964#M9402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I started a project to learn programming in C..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I decided to use the HC08GZ16.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I designed a board for some inputs, outputs and the pull up's &amp;amp; down's for entering monitor mode..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could programm the flash and so on.. all worked fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but then I decided to change from GZ16 up to GZ32.. cause they are pin-compatible!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After brazing the GZ32 on my board i wanted to programm the flash..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It worked fine too, but then after programming the flash the programmer tries to reset the target..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and that's my problem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;it doesn't work.. &lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif"&gt;&lt;IMG alt=":smileyindifferent:" class="emoticon emoticon-smileyindifferent" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif" title="Smiley Indifferent" /&gt;&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Error Message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Attempting to reset target device ... Unsucessfull"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But before programming the flash, the same (i think its the same method to reset) reset works?!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use MON08 - Class 3 to connect to my board!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps someone could help me..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;with best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sascha.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2007 17:34:58 GMT</pubDate>
    <dc:creator>monXii</dc:creator>
    <dc:date>2007-10-29T17:34:58Z</dc:date>
    <item>
      <title>Problem by resetting the HC08GZ32 with MON08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158964#M9402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I started a project to learn programming in C..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I decided to use the HC08GZ16.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I designed a board for some inputs, outputs and the pull up's &amp;amp; down's for entering monitor mode..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could programm the flash and so on.. all worked fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but then I decided to change from GZ16 up to GZ32.. cause they are pin-compatible!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After brazing the GZ32 on my board i wanted to programm the flash..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It worked fine too, but then after programming the flash the programmer tries to reset the target..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and that's my problem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;it doesn't work.. &lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif"&gt;&lt;IMG alt=":smileyindifferent:" class="emoticon emoticon-smileyindifferent" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif" title="Smiley Indifferent" /&gt;&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Error Message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Attempting to reset target device ... Unsucessfull"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But before programming the flash, the same (i think its the same method to reset) reset works?!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use MON08 - Class 3 to connect to my board!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps someone could help me..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;with best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sascha.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2007 17:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158964#M9402</guid>
      <dc:creator>monXii</dc:creator>
      <dc:date>2007-10-29T17:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problem by resetting the HC08GZ32 with MON08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158965#M9403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello and welcome to the forums Sacha,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Class 3 connection does not have any host controlled reset or power control circuitry, so the attempted automatic reset will fail.&lt;/DIV&gt;&lt;DIV&gt;Then the manual power control dialog should pop up. Does it connect after this?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also, are you saying that it worked once but now that you have programmed it you can't connect?&lt;/DIV&gt;&lt;DIV&gt;There are more siganls that need to be correct for a programmed part compared to a blank one.&lt;/DIV&gt;&lt;DIV&gt;Refer to the Monitor or Development paragraph in the datasheet.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2007 18:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158965#M9403</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-10-29T18:11:34Z</dc:date>
    </item>
    <item>
      <title>Re: Problem by resetting the HC08GZ32 with MON08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158966#M9404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;ah.. it doesn't have any automatic reset's..&lt;BR /&gt;so, when i start the programming action wind pops on.. pls push reset button..&lt;BR /&gt;i do this and all works fine!&lt;BR /&gt;and i can programm the flash anytime, cause i use the normal monitor mode, not the force mode..&lt;BR /&gt;&lt;BR /&gt;but when i click my reset button he wrotes "Attempt to reset target device ... Sucessfull"&lt;BR /&gt;then he programm the flash..&lt;BR /&gt;and then i comes again.. "Attempt to reset target device ... Unsucessfull"&lt;BR /&gt;&lt;BR /&gt;and with my GZ16 it works..&lt;BR /&gt;&lt;BR /&gt;but when you say that's normal.. ok &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;BR /&gt;thanks for fast answer!&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2007 18:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-by-resetting-the-HC08GZ32-with-MON08/m-p/158966#M9404</guid>
      <dc:creator>monXii</dc:creator>
      <dc:date>2007-10-29T18:26:24Z</dc:date>
    </item>
  </channel>
</rss>