<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08DZ60CLC Sector Erase Time</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158707#M9372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The required FCDIV setting will depend on the bus frequency you are using - the divider setting must be such that a flash clock frequency within the range 150-200 kHz is generated. A divider setting of 5 will produce a division ratio of 6, implying that the bus clock is within the range 0.9-1.2 MHz.&amp;nbsp; However, I would suspect that this is probably not the case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, if the bus frequency were 8 MHz, a divider setting of decimal 39 would be necessary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 05 Dec 2009 06:11:02 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2009-12-05T06:11:02Z</dc:date>
    <item>
      <title>MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158704#M9369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My application requires a fast sector erase/write time to function as a counter.&amp;nbsp; The measured erase/write time on my MC9S08DZ60CLC has been consistently about 3ms, however, the datasheet&amp;nbsp;(p. 53) states that a sector erase by itself takes 20ms.&amp;nbsp; How is this possible?&amp;nbsp; Did I miss&amp;nbsp;something or does the microcontroller perform better than&amp;nbsp;it's supposed to?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Dec 2009 06:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158704#M9369</guid>
      <dc:creator>rsheldon</dc:creator>
      <dc:date>2009-12-02T06:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158705#M9370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like something is wrong with FCDIV setting. Timing is shorter almost 8 times, as if PRDIV8 bit was not set...&amp;nbsp;Did you note that according to DZ60 datasheet FCDIV is write once register? This means you can't set up DIV5:0 bits first, and then set up PRDIV8 bit. All FCDIV bits should be written at once.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Dec 2009 13:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158705#M9370</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2009-12-02T13:00:35Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158706#M9371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I should explain also that I am just learning assembly language and am trying to understand how a former employee coded our chip.&amp;nbsp; With that said, I took a look at the code and I found one line containing FCDIV that reads as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$05 ;#$45&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;#$05 is for low&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FCDIV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Set clock divider&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this is useful information, if not let me know and I can scrounge up some more code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2009 04:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158706#M9371</guid>
      <dc:creator>rsheldon</dc:creator>
      <dc:date>2009-12-05T04:52:09Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158707#M9372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The required FCDIV setting will depend on the bus frequency you are using - the divider setting must be such that a flash clock frequency within the range 150-200 kHz is generated. A divider setting of 5 will produce a division ratio of 6, implying that the bus clock is within the range 0.9-1.2 MHz.&amp;nbsp; However, I would suspect that this is probably not the case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, if the bus frequency were 8 MHz, a divider setting of decimal 39 would be necessary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2009 06:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158707#M9372</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-12-05T06:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158708#M9373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This appears to be the section of code in question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;;;; Drop down to 4MHz&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; MCGC2: BDIV=0,RANGE=0,HGO=0,LP=0,EREFS=0,ERCLKEN=0,EREFSTEN=0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;CLR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCGC2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Set MCGC2 register&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$40,MCGC2&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; MCGC1: CLKS=0,RDIV=4,IREFS=1,IRCLKEN=1,IREFSTEN=0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$1E,MCGC1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;#$26 for low #$06 for high&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; MCGC3: LOLIE=0,PLLS=0,CME=0,VDIV=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$01,MCGC3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Set MCGC3 register&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; ### Init_FLASH init code&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; FSTAT: FCBEF=0,FCCF=0,FPVIOL=1,FACCERR=1,FBLANK=0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #%00110000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FSTAT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Clear error flags&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$05 ;#$45&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;#$05 is for low&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FCDIV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Set clock divider&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks as if he loaded the accumulator with 0x05 and stored that value in FCDIV, but the comment shows he's setting FCDIV as 0x19. Am I interpreting this correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2009 04:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158708#M9373</guid>
      <dc:creator>rsheldon</dc:creator>
      <dc:date>2009-12-16T04:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60CLC Sector Erase Time</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158709#M9374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would appear that the code you have posted has been generated by the PE initialisation tool.&amp;nbsp; However, the FCDIV setting has then been altered without the comment line being updated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp; ; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #$05 ;#$45&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;#$05 is for low&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FCDIV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Set clock divider&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The original PE initialisation gives a value of $29 (decimal 41) for a division ratio of 42.&amp;nbsp; With this value, a trimmed bus frequency of nominally 8 MHz would give a flash clock frequency of 190 kHz, which makes allowance for a bus frequency tolerance of +/-5%. (This allowance would not be necessary if an external crystal reference were utilised.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Accepting that the new bus frequency has been trimmed to 4 MHz, and allowing a similar frequency tolerance, the required division ratio would be 21.&amp;nbsp; Therefore the FCDIV setting should be $14 (20 decimal).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suggest that you check the MCG register settings to determine whether the bus frequency is actually 4.0 MHz, as the initial comment suggests.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2009 11:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60CLC-Sector-Erase-Time/m-p/158709#M9374</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-12-16T11:13:44Z</dc:date>
    </item>
  </channel>
</rss>