<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158046#M9258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a number of design issues associated with your analog measurement requirements.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will first need to determine the analog interface circuitry required, which may extend beyond a simple voltage divider.&amp;nbsp; If the analog signals originate from the "outside world" you will surely need to protect the MCU against high voltage transients.&amp;nbsp; Additionally you will need to consider the source resistance of these signals - to achieve sufficient accuracy in conjunction with12-bit resolution, the signals&amp;nbsp;will each need to&amp;nbsp;provide a low source resistance to each ADC input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;More than likely additional voltage follower buffers would be necessary, to be interspersed between the voltage divider and the ADC input.&amp;nbsp;&amp;nbsp;The voltage divider would need to be of sufficiently high resistance for negligible loading of the source, dictating the use of operational amplifiers with very low input bias current.&amp;nbsp; Without knowing the nature of the signal sources, I cannot be any more specific.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The initial accuracy of the voltage divider components can be compensated for if a calibration process occurs during production,&amp;nbsp;so that correction factors can be determined and stored.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the smaller pin count MCUs, the ADC reference will be internally tied to the Vdd and Vss rails.&amp;nbsp; Any variation of the supply voltage, with temperature or load, will affect the accuracy of the measurements.&amp;nbsp; It is possible to compensate for long term Vdd variations by also measuring&amp;nbsp;a separate internal bandgap reference within the MCU.&amp;nbsp; You will need to determine whether the Vdd supply rail is sufficiently stable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since all MCUs generate internal noise, this can cause problems, especially for 12-bit conversions.&amp;nbsp; One possible approach is to put the MCU into lower power wait mode immediately after a conversion is started, and then use the ADC interrupt to wakeup and read the result.&amp;nbsp; Another&amp;nbsp;method might be to take multiple readings of each signal, and use the average result.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you cannot achieve the desired accuracy using the internal ADC module, you might need to use an external ADC device that communicates to the MCU, typically via SPI.&amp;nbsp; This can be used inconjunction with an accurate external voltage reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Oct 2010 00:43:10 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-10-27T00:43:10Z</dc:date>
    <item>
      <title>cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158042#M9254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is my first post.&lt;/P&gt;&lt;P&gt;When looking for an 8 bits microcontroler with 2 ADC (12bit) I always arrive to the S08LC family:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DS08LC%26fsrch%3D1%26sr%3D1" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08LC&amp;amp;fsrch=1&amp;amp;sr=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is that I want a simple microcontroller, not with 64 pins!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, is there any 16 pins (more or less) microcontroller with 2 ch ADC and 1 UART for transmiting RS232 to a PC?&lt;/P&gt;&lt;P&gt;Also want to use C programming&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope to hear some solution.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Oct 2010 04:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158042#M9254</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-26T04:16:13Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158043#M9255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check out the MC9S08QE8 series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Oct 2010 07:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158043#M9255</guid>
      <dc:creator>marbomb</dc:creator>
      <dc:date>2010-10-26T07:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158044#M9256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good, MC9S08QE8 and MC9s08QB8 seems to fit the requirements, both of them has 12 bit-ADC and SCI for RS232 (PC). My main problem is that these are low power consumption (3.6V power supply).&lt;/P&gt;&lt;P&gt;I have two 0-5V analog signals to plug into the microcontroller. And In pages 25 and 20 respectively of:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;QE8&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08QE8.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08QE8.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;QB8&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08QB8.pdf?pspll=1" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08QB8.pdf?pspll=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;tells that the input signal of the analog source cannot go higher than Vdd...&lt;/P&gt;&lt;P&gt;This 5V signals are read as XXX.X value, (max value: 199.9) -&amp;gt; that is 200*10 = 2000 possible values (0-5)V. The tolerance is around 0.1%. Im afraid to try the conversion 5V to 3.3V cause the increment of the tolerance... I cannot permit any tolerance even in decimal values.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PIC18F2423 is knocking at the door, but I once used freescale and codewarrior and thought give it a try in my next project. But it seems 12 bit ADC only applies to ultralow power consumption...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to use freescale but I have this ultra low power consumption problem :s&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;¿better to use PIC for this case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cheers from Spain&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Oct 2010 19:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158044#M9256</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-26T19:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158045#M9257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Conversion from 5V to 3.3V can be done with a resistive divisor of (0.1%) tolerance resistances, that is true. What I fear is the noise for 2000 values.&lt;/P&gt;&lt;P&gt;With 5 V&amp;nbsp; -&amp;gt;&amp;nbsp; 1 step in the ADC in milivolts would be 5000mv / 2000values = 2.5 mv = 1 step&lt;/P&gt;&lt;P&gt;with 3.6V -&amp;gt; 1.8mv = 1 step&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Considering that 'this' is the solution, (dont see another way to do it) I´ve seen the starter kit DEMO9S08QE8 as a quick way to see if the software works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I safely use this solution? Just I would like to hear your opinion just in case Im missing something...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Oct 2010 20:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158045#M9257</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-26T20:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158046#M9258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a number of design issues associated with your analog measurement requirements.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will first need to determine the analog interface circuitry required, which may extend beyond a simple voltage divider.&amp;nbsp; If the analog signals originate from the "outside world" you will surely need to protect the MCU against high voltage transients.&amp;nbsp; Additionally you will need to consider the source resistance of these signals - to achieve sufficient accuracy in conjunction with12-bit resolution, the signals&amp;nbsp;will each need to&amp;nbsp;provide a low source resistance to each ADC input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;More than likely additional voltage follower buffers would be necessary, to be interspersed between the voltage divider and the ADC input.&amp;nbsp;&amp;nbsp;The voltage divider would need to be of sufficiently high resistance for negligible loading of the source, dictating the use of operational amplifiers with very low input bias current.&amp;nbsp; Without knowing the nature of the signal sources, I cannot be any more specific.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The initial accuracy of the voltage divider components can be compensated for if a calibration process occurs during production,&amp;nbsp;so that correction factors can be determined and stored.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the smaller pin count MCUs, the ADC reference will be internally tied to the Vdd and Vss rails.&amp;nbsp; Any variation of the supply voltage, with temperature or load, will affect the accuracy of the measurements.&amp;nbsp; It is possible to compensate for long term Vdd variations by also measuring&amp;nbsp;a separate internal bandgap reference within the MCU.&amp;nbsp; You will need to determine whether the Vdd supply rail is sufficiently stable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since all MCUs generate internal noise, this can cause problems, especially for 12-bit conversions.&amp;nbsp; One possible approach is to put the MCU into lower power wait mode immediately after a conversion is started, and then use the ADC interrupt to wakeup and read the result.&amp;nbsp; Another&amp;nbsp;method might be to take multiple readings of each signal, and use the average result.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you cannot achieve the desired accuracy using the internal ADC module, you might need to use an external ADC device that communicates to the MCU, typically via SPI.&amp;nbsp; This can be used inconjunction with an accurate external voltage reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 00:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158046#M9258</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-27T00:43:10Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158047#M9259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, the source is a current source&amp;nbsp; passing through resistances. So the output impedance in the 'source box' is very low ... aprox 100 ohms. thats necesary to get 0-5V from the current source.&lt;/P&gt;&lt;P&gt;And Yes, it can be calibrated, but the point is that the voltage is applied to an LCD for measurement... The reference of 5V comes from a regulator. (dont remember the name of the chip right now... TRACO?...yes a traco power.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the voltage divisor needs a potentiometer ... -&amp;gt; high tolerance&lt;/P&gt;&lt;P&gt;or some trick with reference voltage and the ADC...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems like im going to spend more time in the ADC than anything...&lt;/P&gt;&lt;P&gt;Thank you for the answers. I will use PIC &lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope to use freescale next time&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All the Best&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 01:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158047#M9259</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-27T01:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158048#M9260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="color: #000000;"&gt;You can choose MC9S08DZ16ACLC or&lt;/SPAN&gt;&lt;/SPAN&gt; MC9S08MP12VWL&lt;SPAN&gt;&lt;SPAN style="color: #000000;"&gt;, it has a better cost performance than the PIC18F2423.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 01:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158048#M9260</guid>
      <dc:creator>Mickey</dc:creator>
      <dc:date>2010-10-27T01:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158049#M9261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cris,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many of the problem areas that I mentioned will apply generally to 12-bit measurements, whether you are using Freescale or PIC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the input signals are derived from constant current sources, the simplest approach would be to adjust the load resistances, currently 100 ohms, to a proportionally lower value for 3.3 volt full scale.&amp;nbsp; It may still be useful to use unity gain buffers, to isolate the inputs of the MCU, and effectively provide transient voltage protection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 01:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158049#M9261</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-27T01:52:01Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158050#M9262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mac I will study that, I was thinking about inserting an insolator, I dont realized of the transients, jojo. About the voltage divider to get the 3.3V is clear, but I will try to avoid a 3.3V for the moment unless there isn´t another way. Much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="color: #000000;"&gt;MC9S08DZ16ACLC ... I´m going to put an eye in this. Tomorrow more. Thanks!&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 02:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158050#M9262</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-27T02:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: cant find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158051#M9263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Betadine,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the JM family has 5V and 12 Bit ADC and is available in QFP32, still not large.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 16:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158051#M9263</guid>
      <dc:creator>Obetz</dc:creator>
      <dc:date>2010-10-27T16:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: can't find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158052#M9264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="color: #000000;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt; Obetz, the JM family is a nice shot. Instead it has problems for Full speed USB applications, Ive read that for slow communications it works good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I´m considering finally to buy the DEMO9S08JM16 (cause I haven't touch any microcontroller since 2 years) so I need newbie first steps to test the software)&lt;/P&gt;&lt;P&gt;Now comes the big question with this demo board:&lt;/P&gt;&lt;P&gt;Is it really possible to make a RS-232 bridge through USB with this demoboard?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I need is to test a serial RS-232 COM communication through USB, I can do it with a TUSB or something that converts it independently of the micro, I know, but i would like to see if the 'marvelous'&amp;nbsp; VBA for Excel can really establish a serial RS-232 communication with a USB (RS232 protocol). If it works, the I will design something in Altium for finally release the converter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, It would be nice if the demo board brings code examples to use RS232 with and without USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Will I receive code examples for quickly test a 'hello world' or do I have to search through web?&lt;/P&gt;&lt;P&gt;Thanks for all for the suggestions!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PD: Mac I will let you know how the 12bit ADC goes.&lt;/P&gt;&lt;P&gt;PD: The packager is not a problem, since the creation of flux you can solder the small pins without problems. One piece of flux, solder and fsssshhhh all pins get sold without shortcircuits, (not always work)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Oct 2010 20:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158052#M9264</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-27T20:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: can't find a 2ch 12bit ADC simple microcontroller...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158053#M9265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well It´s done, I bought the demo kit, hope to achieve the rs-232 connection through USB. It seems that it brings software examples and applications for that purpose. Thank you for the orientation to all. Let´s see how the JM family works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Oct 2010 20:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/cant-find-a-2ch-12bit-ADC-simple-microcontroller/m-p/158053#M9265</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-10-28T20:32:33Z</dc:date>
    </item>
  </channel>
</rss>