<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Freescale 802.15.4 MAC???</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157443#M9166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;2. the second packet will be discard by the MAC layer,because those two packets have the same sequence number.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 08 Mar 2009 14:54:47 GMT</pubDate>
    <dc:creator>xiaof</dc:creator>
    <dc:date>2009-03-08T14:54:47Z</dc:date>
    <item>
      <title>Freescale 802.15.4 MAC???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157440#M9163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have bassically two questions about the full (not the SMAC) Freescale 802.15.4 MAC:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is there a way to know how many MAC retries has been used to transmit a message?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. If a radio receive two times the same packet (in the case the&amp;nbsp; first ack was send but not receive by the transmitter), is the second packet discard by the MAC layer? If not, is there a way to have access to the sequence number of the received packet?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help!&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2009 02:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157440#M9163</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-02-28T02:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale 802.15.4 MAC???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157441#M9164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Anyone understanding these issues?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2009 22:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157441#M9164</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-03-04T22:42:50Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale 802.15.4 MAC???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157442#M9165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. retries times is &amp;nbsp;a MAC constant:aMaxFrameRetries,it's value is 3.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2009 20:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157442#M9165</guid>
      <dc:creator>xiaof</dc:creator>
      <dc:date>2009-03-07T20:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale 802.15.4 MAC???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157443#M9166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;2. the second packet will be discard by the MAC layer,because those two packets have the same sequence number.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2009 14:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-802-15-4-MAC/m-p/157443#M9166</guid>
      <dc:creator>xiaof</dc:creator>
      <dc:date>2009-03-08T14:54:47Z</dc:date>
    </item>
  </channel>
</rss>