<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: network-S08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126064#M903</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;To get a module like this on S08, I would suggest you use the "Design your own MCU" feature on FSL website.&lt;BR /&gt; I suppose your suggestion will be relayed to the appropriate person.&lt;BR /&gt;&lt;BR /&gt;However, I'm not quite sure this kind of MCU is big enough to be very attractive. I mean, already on the NE64 EVB, some external RAM was added.&amp;nbsp; (you can see some posts on the forum from people interfacing it)&lt;BR /&gt;You'll probably need a bit more RAM and 64KB-Flash offered by the S08 today to run a server.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;May be a module to send alerts without being a server could be small enough to fit in an S08. But if you've got the Ethernet ability I'm pretty sure you'll want to use it to flash over Ethernet and also configure via the network.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Which means more memory...&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Alban.&lt;/FONT&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2006 23:54:49 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2006-02-15T23:54:49Z</dc:date>
    <item>
      <title>network-S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126061#M900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;since the latest HCS08AW is now&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;available with 5volt and 20MHz,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;is it possible to introduce a network&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TCP/IP module in S08 engine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(we don't want to migrate to S12NE64)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2006 16:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126061#M900</guid>
      <dc:creator>devakotcha</dc:creator>
      <dc:date>2006-02-08T16:37:37Z</dc:date>
    </item>
    <item>
      <title>Re: network-S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126062#M901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Hi,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Are you talking about an internal module in the following series or you want to interface an existing Ethernet module ?&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Cheers,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Alban.&lt;/FONT&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2006 00:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126062#M901</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-02-10T00:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: network-S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126063#M902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;we are talking about an internal module in&lt;BR /&gt;the following series like NE64 of 16bit&lt;BR /&gt;we need a TCP/IP inside a HCS08 chip&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2006 13:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126063#M902</guid>
      <dc:creator>devakotcha</dc:creator>
      <dc:date>2006-02-15T13:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: network-S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126064#M903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;To get a module like this on S08, I would suggest you use the "Design your own MCU" feature on FSL website.&lt;BR /&gt; I suppose your suggestion will be relayed to the appropriate person.&lt;BR /&gt;&lt;BR /&gt;However, I'm not quite sure this kind of MCU is big enough to be very attractive. I mean, already on the NE64 EVB, some external RAM was added.&amp;nbsp; (you can see some posts on the forum from people interfacing it)&lt;BR /&gt;You'll probably need a bit more RAM and 64KB-Flash offered by the S08 today to run a server.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;May be a module to send alerts without being a server could be small enough to fit in an S08. But if you've got the Ethernet ability I'm pretty sure you'll want to use it to flash over Ethernet and also configure via the network.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Which means more memory...&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Alban.&lt;/FONT&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2006 23:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/network-S08/m-p/126064#M903</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-02-15T23:54:49Z</dc:date>
    </item>
  </channel>
</rss>