<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックneed some advice</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-some-advice/m-p/156601#M9022</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been given the task of updating a two-way radio that my company produces.&amp;nbsp; Currently we use the&lt;/P&gt;&lt;P&gt;MC68HC908AP32.&amp;nbsp; Should I keep using it or update to a new one that is HCS08?&amp;nbsp; I need to get about 5 more years of production and I am worried the MC68HC908AP32 wont be around.&amp;nbsp; And what would be a good replacment?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Oct 2010 22:29:17 GMT</pubDate>
    <dc:creator>mikeradio</dc:creator>
    <dc:date>2010-10-20T22:29:17Z</dc:date>
    <item>
      <title>need some advice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-some-advice/m-p/156601#M9022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been given the task of updating a two-way radio that my company produces.&amp;nbsp; Currently we use the&lt;/P&gt;&lt;P&gt;MC68HC908AP32.&amp;nbsp; Should I keep using it or update to a new one that is HCS08?&amp;nbsp; I need to get about 5 more years of production and I am worried the MC68HC908AP32 wont be around.&amp;nbsp; And what would be a good replacment?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Oct 2010 22:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/need-some-advice/m-p/156601#M9022</guid>
      <dc:creator>mikeradio</dc:creator>
      <dc:date>2010-10-20T22:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: need some advice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-some-advice/m-p/156602#M9023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your concerns are probably warranted since the device you are using is currently classified "not recommended for new design".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The choice of a new 8-bit MCU type from the more recent 9S08 family will probably depend on which of the more "exotic" features of the current MCU that you are actually using.&amp;nbsp; Within this category I would place -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The IR encoder/decoder operation associated with one of the SCI modules.&lt;/LI&gt;&lt;LI&gt;The IRQ2 input pin.&lt;/LI&gt;&lt;LI&gt;The 25mA open drain output pins.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;It is also unclear to me how the SMBus requirements differ from standard IIC module operation, should you make use of this feature.&amp;nbsp; You will also need to consider whether a FLL can replace a PLL for your application.&amp;nbsp; The FLL will have considerably more short term phase&amp;nbsp;jitter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The TBM functionality for the current device might be substitued by&amp;nbsp;an RTC module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another important consideration would be whether the scope of the product re-design can accommodate 3.3 volt operation in lieu of 5 volt operation.&amp;nbsp; If not, this would limit the MCU choice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As a starting point, you might consider the 9S08ACxx for 5 volt operation, or the 9S08QExx for 3.3 volt operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Oct 2010 17:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/need-some-advice/m-p/156602#M9023</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-21T17:55:33Z</dc:date>
    </item>
  </channel>
</rss>