<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: HC08LK code size problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156450#M8997</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hossam,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the HC908LK24 device was originally chosen because of its LCD drive capability, you might wish to examine the datasheet for the more recent HCS08LC60.&amp;nbsp; This is a member of the newer HCS08 family.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have not compared the two pinouts, but I suspect that it will be quite unlikely that they are similar to each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With regard to coding, that associated with all on-chip peripherals will certainly need to be modified, to be consistent with the register naming, and for compatibility with the operation details of each peripheral.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Feb 2009 17:23:51 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2009-02-26T17:23:51Z</dc:date>
    <item>
      <title>HC08LK code size problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156449#M8996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am uing HC08LK family.&lt;/P&gt;&lt;P&gt;Now my code size exceeds the 24K Flash.&lt;/P&gt;&lt;P&gt;Is there any rplacment with more flash size 32K or 64K.&lt;/P&gt;&lt;P&gt;I am looking for the replacemnt micro which requires the least changes in my source code and HW design&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Hossam Alzomor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2009 13:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156449#M8996</guid>
      <dc:creator>alzomor</dc:creator>
      <dc:date>2009-02-26T13:07:22Z</dc:date>
    </item>
    <item>
      <title>Re: HC08LK code size problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156450#M8997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hossam,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the HC908LK24 device was originally chosen because of its LCD drive capability, you might wish to examine the datasheet for the more recent HCS08LC60.&amp;nbsp; This is a member of the newer HCS08 family.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have not compared the two pinouts, but I suspect that it will be quite unlikely that they are similar to each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With regard to coding, that associated with all on-chip peripherals will certainly need to be modified, to be consistent with the register naming, and for compatibility with the operation details of each peripheral.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2009 17:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156450#M8997</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-02-26T17:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: HC08LK code size problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156451#M8998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mac,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any Application note for megiration from LK24 to LC60?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Hossam Alzomor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2009 01:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156451#M8998</guid>
      <dc:creator>alzomor</dc:creator>
      <dc:date>2009-02-27T01:22:53Z</dc:date>
    </item>
    <item>
      <title>Re: HC08LK code size problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156452#M8999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hossam,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am unfamiliar with the application notes that may pertain to the 'LC60.&amp;nbsp; However, if you examine the products section of the Freescale website, you can drill down to the webpage containing specific information about the 'LC60 device.&amp;nbsp; Here you will generally find a list of all the application notes that pertain to that product, and can download the documents from that webpage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2009 06:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08LK-code-size-problem/m-p/156452#M8999</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-02-27T06:58:41Z</dc:date>
    </item>
  </channel>
</rss>