<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Motorola MCU's from Seagate HDD's - need identify</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156228#M8974</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many of the sub-gigabyte Conner drives had some version of a 68HC11A or -E on them: this is from personal experience. I have _heard_ that some had 68HC16s and 68HC11Fs.&lt;/P&gt;&lt;P&gt;The HC11A-types had an internal ROM, but it was not used. Many of those I looked at (20 or so) had a version of the BUFFALO monitor on board and a very few had (presumably non-functional) Chrysler Corporation engine-control code. Those with the BUFFALO-monitor can be brought up with the super-special monitor connection (Vague, I know:It's been a long time) and reprogrammed to boot the monitor. Those without the monitor can be used to execute a 256-byte program from EEPROM.&lt;/P&gt;&lt;P&gt;Most of them ran at 2MHz bus-clock and a few later ones at 3MHz.&lt;/P&gt;&lt;P&gt;It would be quite a bit of work to exploit these. The amount of fun is up to you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wade Hassler&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Nov 2010 03:33:29 GMT</pubDate>
    <dc:creator>WadeH</dc:creator>
    <dc:date>2010-11-15T03:33:29Z</dc:date>
    <item>
      <title>Motorola MCU's from Seagate HDD's - need identify</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156225#M8971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i need identify some Motorola MCU's from older Conner /Seagate HDD's. I need know identify as MC68HC part:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SC415016AFU 0E87J&lt;/P&gt;&lt;P&gt;SC415016AFU 0E61H&lt;/P&gt;&lt;P&gt;SC415016CFU 0F17V&lt;/P&gt;&lt;P&gt;SC415111FU 3C94R&lt;/P&gt;&lt;P&gt;SC416880FU 1G24M&lt;/P&gt;&lt;P&gt;SC416880FU 0G79C&lt;/P&gt;&lt;P&gt;SC439566FU8 0G14T&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you can help me someone, very please?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Very thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Oct 2010 20:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156225#M8971</guid>
      <dc:creator>Worfvx</dc:creator>
      <dc:date>2010-10-19T20:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: Motorola MCU's from Seagate HDD's - need identify</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156226#M8972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;im afraid you wont get answer&lt;/P&gt;&lt;P&gt;its probably part of NDA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if you are sure its mc68h part maybe you could try to read the info you can inside the chip maybe its model is there&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Oct 2010 20:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156226#M8972</guid>
      <dc:creator>Juls</dc:creator>
      <dc:date>2010-10-21T20:14:54Z</dc:date>
    </item>
    <item>
      <title>Re: Motorola MCU's from Seagate HDD's - need identify</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156227#M8973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;inside the chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Oct 2010 01:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156227#M8973</guid>
      <dc:creator>Worfvx</dc:creator>
      <dc:date>2010-10-22T01:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: Motorola MCU's from Seagate HDD's - need identify</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156228#M8974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many of the sub-gigabyte Conner drives had some version of a 68HC11A or -E on them: this is from personal experience. I have _heard_ that some had 68HC16s and 68HC11Fs.&lt;/P&gt;&lt;P&gt;The HC11A-types had an internal ROM, but it was not used. Many of those I looked at (20 or so) had a version of the BUFFALO monitor on board and a very few had (presumably non-functional) Chrysler Corporation engine-control code. Those with the BUFFALO-monitor can be brought up with the super-special monitor connection (Vague, I know:It's been a long time) and reprogrammed to boot the monitor. Those without the monitor can be used to execute a 256-byte program from EEPROM.&lt;/P&gt;&lt;P&gt;Most of them ran at 2MHz bus-clock and a few later ones at 3MHz.&lt;/P&gt;&lt;P&gt;It would be quite a bit of work to exploit these. The amount of fun is up to you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wade Hassler&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Nov 2010 03:33:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156228#M8974</guid>
      <dc:creator>WadeH</dc:creator>
      <dc:date>2010-11-15T03:33:29Z</dc:date>
    </item>
    <item>
      <title>Re: Motorola MCU's from Seagate HDD's - need identify</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156229#M8975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your help, Wade H. I have some HDD's boards in photos. I can send this photos to you for better exact identification. Do you can make this for me? I need also identify MCU on some others HDD boards, example Seagate ST-251.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Nov 2010 04:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Motorola-MCU-s-from-Seagate-HDD-s-need-identify/m-p/156229#M8975</guid>
      <dc:creator>Worfvx</dc:creator>
      <dc:date>2010-11-15T04:48:54Z</dc:date>
    </item>
  </channel>
</rss>