<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: unique identification of device - HCS08DZ60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156001#M8921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I use the DZ60 too. I have a CAN Bootloader. As well as being able to load application firmware, it's also able to write a serial number to flash. We use the serial number to "randomise" the CAN device number, so that it's unique on the CANbus. The device number is stored in EEprom, so there's no hardware switch settings&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 May 2008 18:19:02 GMT</pubDate>
    <dc:creator>Bruce_andrew</dc:creator>
    <dc:date>2008-05-18T18:19:02Z</dc:date>
    <item>
      <title>unique identification of device - HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/155999#M8919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Dear all!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've got the following question: Is there any possibility to uniquely identify a HCS08 device? I.e. is there any register, or serial number that I could somehow read out by SW?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In one system I'm using&amp;nbsp; 5 to 10 devices for which I want to use the same SW, but the devices have to use different&amp;nbsp; IDs for CAN-communication. If possible I want to avoid a solution in HW (dip-switch or so) because of space available and cost issues...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any possibility to get a&amp;nbsp; different data (e.g. serial num)&amp;nbsp; from each uC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the HCS08DZ60 devices.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your ideas, hints and tips,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Johannes&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Added p/n to subject.&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-05-15&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;07:41 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2008 18:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/155999#M8919</guid>
      <dc:creator>ohanica</dc:creator>
      <dc:date>2008-05-15T18:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: unique identification of device - HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156000#M8920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Johannes,&lt;BR /&gt;&lt;BR /&gt;No there is nothing "hard coded" into the device that is in anyway unique.&lt;BR /&gt;You would have to do it yourself, perhaps using something like &lt;A href="https://www.pemicro.com/login.cfm?from_url=http://www.pemicro.com/downloads/download_file.cfm?download_id=102" rel="nofollow" target="_blank"&gt;P&amp;amp;E's Serialise&lt;/A&gt; programme.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2008 05:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156000#M8920</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-05-16T05:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: unique identification of device - HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156001#M8921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I use the DZ60 too. I have a CAN Bootloader. As well as being able to load application firmware, it's also able to write a serial number to flash. We use the serial number to "randomise" the CAN device number, so that it's unique on the CANbus. The device number is stored in EEprom, so there's no hardware switch settings&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 May 2008 18:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156001#M8921</guid>
      <dc:creator>Bruce_andrew</dc:creator>
      <dc:date>2008-05-18T18:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: unique identification of device - HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156002#M8922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Bruce!&lt;BR /&gt;&lt;BR /&gt;thats a good idea, to use the bootloader to program some data (serial number) into the EEPROM. This might be quiet interesting for me, but it is still not completely satisfying cause I need to tell the bootloader which number to write in each device... So I still have to make this decision somehow by myself; but the idea is already better than coding something in HW. I'll think about it, maybe I can adapt it to my prject.&lt;BR /&gt;&lt;BR /&gt;thanks and regards,&lt;BR /&gt;Johannes&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 May 2008 20:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/unique-identification-of-device-HCS08DZ60/m-p/156002#M8922</guid>
      <dc:creator>ohanica</dc:creator>
      <dc:date>2008-05-19T20:23:42Z</dc:date>
    </item>
  </channel>
</rss>