<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Using USB Multilink MON08 for HC908GP32</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-USB-Multilink-MON08-for-HC908GP32/m-p/155961#M8911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MY,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has been awhile since I made a MON08 interface for a GP32.&amp;nbsp; As I recall there are 3 pins which must be in the correct state when the reset pin goes inactive.&amp;nbsp; These pins specify the baud rate, baud rate source, and boot mode of the GP32.&amp;nbsp; If the boot mode is MON08 then the GP32 will be available to connect serially using pin PTA0 to your MON08 host and receive commands.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a schematic of a GP32 production board I made and attached it to this response.&amp;nbsp; As you can see, when the CPU08 programmer is attached, the PA7 and PC1 pins are pulled low and the PC0 and PC3 pins are pulled high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In production none of the diodes were stuffed and a bed of nails fixture was used for program and test.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good Luck,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Apr 2012 20:36:10 GMT</pubDate>
    <dc:creator>PeterHouse</dc:creator>
    <dc:date>2012-04-20T20:36:10Z</dc:date>
    <item>
      <title>Using USB Multilink MON08 for HC908GP32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-USB-Multilink-MON08-for-HC908GP32/m-p/155960#M8910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am having some problem entering debugging mode using MON08 on GP32 but I manage to do it for AB32.&lt;/P&gt;&lt;P&gt;Can Anyone give any advise?&lt;/P&gt;&lt;P&gt;I have also attached some pictures of my PCB debug pin connection and my mon08 connection pictures.&lt;/P&gt;&lt;P&gt;Please advise.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2012 14:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-USB-Multilink-MON08-for-HC908GP32/m-p/155960#M8910</guid>
      <dc:creator>mylim</dc:creator>
      <dc:date>2012-04-20T14:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using USB Multilink MON08 for HC908GP32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-USB-Multilink-MON08-for-HC908GP32/m-p/155961#M8911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MY,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has been awhile since I made a MON08 interface for a GP32.&amp;nbsp; As I recall there are 3 pins which must be in the correct state when the reset pin goes inactive.&amp;nbsp; These pins specify the baud rate, baud rate source, and boot mode of the GP32.&amp;nbsp; If the boot mode is MON08 then the GP32 will be available to connect serially using pin PTA0 to your MON08 host and receive commands.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a schematic of a GP32 production board I made and attached it to this response.&amp;nbsp; As you can see, when the CPU08 programmer is attached, the PA7 and PC1 pins are pulled low and the PC0 and PC3 pins are pulled high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In production none of the diodes were stuffed and a bed of nails fixture was used for program and test.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good Luck,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2012 20:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-USB-Multilink-MON08-for-HC908GP32/m-p/155961#M8911</guid>
      <dc:creator>PeterHouse</dc:creator>
      <dc:date>2012-04-20T20:36:10Z</dc:date>
    </item>
  </channel>
</rss>