<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Clarification on BKGD connection</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155712#M8852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I read on the forum some where that the Vdd pin on the BKGD connector of the USB-ML-12E is a read pin, so when connecting to a target circuit that uses external power supply the Vdd pin on the BKGD connector is connected to the external power supply also.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this correct???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Nov 2009 12:11:02 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2009-11-19T12:11:02Z</dc:date>
    <item>
      <title>Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155712#M8852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I read on the forum some where that the Vdd pin on the BKGD connector of the USB-ML-12E is a read pin, so when connecting to a target circuit that uses external power supply the Vdd pin on the BKGD connector is connected to the external power supply also.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this correct???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2009 12:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155712#M8852</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-11-19T12:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155713#M8853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes the "V" pin of the connector is a voltage reference, so that you can use the BDM on both 3V and 5V targets.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2009 15:51:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155713#M8853</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2009-11-19T15:51:53Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155714#M8854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Is there a Freescale document that covers this? I can not seem to find anything that talks about this.....&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2009 21:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155714#M8854</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-11-19T21:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155715#M8855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Various app notes like AN3335 for HCS08 or AN2104 for HCS12. Neither provides a definition to what "Vdd" is, however. The implementation of this seems to be pod-specific. Older BDM pods from PE could be supplied by the target from this pin, for example.&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2009 00:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155715#M8855</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2009-11-20T00:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155716#M8856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Learner,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VDD pin on the the USB-ML-12E is indeed an INPUT to the multilink. The USB-ML-12E uses this to determine the logic voltage level of the target processor, which is the logic high voltage required for BKGD and RESET. The USB-ML-12E draws about 1mA of current on this pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Edison&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2009 00:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155716#M8856</guid>
      <dc:creator>EdT</dc:creator>
      <dc:date>2009-11-20T00:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification on BKGD connection</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155717#M8857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much guys for clearing this up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 more question, how did you guys find out about this???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can't say I have read all the information available in relation to the HCS08 and the background debug pod but I certainly have yet to come accross information that clarifies this. Sigh......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been using the USB-ML-12E for some time now and all this time I have been programming my target board with the Vdd pin open, the target board is using external power supply. Recently the USB-ML-12E stopped working and I have requested technical support from both PE and Freescale, both times the technical support requested for my circuit wiring diagram.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After showing them the schematic and described how the pod is connected to my target board, NON of them picked up on this after exchanging many emails.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I SIMPLY CAN NOT BELIEVE IT!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have placed a service request asking this exact question, it has been 4 days now and the Status is still Unassigned at this very moment.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now it seems I have a USB-ML-12E that's not working and there isn't any documents with any clarification about this...... &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sigh.......&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by Learner on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-11-19&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;10:15 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2009 06:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clarification-on-BKGD-connection/m-p/155717#M8857</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-11-20T06:12:53Z</dc:date>
    </item>
  </channel>
</rss>