<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Program Multiple Target Boards</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155692#M8836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You cannot parallel two boards!&amp;nbsp; It is one board at a time connected to a Cyclone,&amp;nbsp;because the BKGD/MS pin utilises data transfer in both directions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The previous comment made referred to the possibility&amp;nbsp;for the Cyclone to operate stand alone,&amp;nbsp;without the need to always be connected to a computer.&amp;nbsp; This would simplify the use of multiple Cyclone Pros, but still only with&amp;nbsp;a single board connected to each one at any instant.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Oct 2010 14:38:52 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-10-21T14:38:52Z</dc:date>
    <item>
      <title>Program Multiple Target Boards</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155689#M8833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are in the production phase and would like to know would it be possible to use either the (one) Cyclone Pro, or USB multilink to program multiple target boards.&amp;nbsp; Or does anyone know of any other products in the market&amp;nbsp; that offer this capability ?&lt;/P&gt;&lt;P&gt;We are using the HCS08 series.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Oct 2010 03:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155689#M8833</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2010-10-16T03:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: Program Multiple Target Boards</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155690#M8834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we use cyclone pro&lt;/P&gt;&lt;P&gt;but its 1 unit programmed by cyclone&lt;/P&gt;&lt;P&gt;but you can get more cyclone&lt;/P&gt;&lt;P&gt;as a standalone its pretty easy&amp;nbsp; you dont need a pc conected to program each unit&lt;/P&gt;&lt;P&gt;only a properly configured cyclone&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Oct 2010 23:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155690#M8834</guid>
      <dc:creator>Juls</dc:creator>
      <dc:date>2010-10-16T23:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Program Multiple Target Boards</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155691#M8835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, i am using the cyclone pro too. I tried to connect two boards in parralel to the cyclone but it didn't&amp;nbsp; work/program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Oct 2010 22:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155691#M8835</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2010-10-20T22:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: Program Multiple Target Boards</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155692#M8836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You cannot parallel two boards!&amp;nbsp; It is one board at a time connected to a Cyclone,&amp;nbsp;because the BKGD/MS pin utilises data transfer in both directions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The previous comment made referred to the possibility&amp;nbsp;for the Cyclone to operate stand alone,&amp;nbsp;without the need to always be connected to a computer.&amp;nbsp; This would simplify the use of multiple Cyclone Pros, but still only with&amp;nbsp;a single board connected to each one at any instant.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Oct 2010 14:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Multiple-Target-Boards/m-p/155692#M8836</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-21T14:38:52Z</dc:date>
    </item>
  </channel>
</rss>