<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 HCS908LL16/36/64, Battery Capacity, Battery Life Calculation Tool.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS908LL16-36-64-Battery-Capacity-Battery-Life-Calculation-Tool/m-p/155283#M8792</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is the authoritative source that gives an AA alkaline cell a capacity of approximately 2800mAh with a 1mA constant load? What did Freescale use for a cutoff&amp;nbsp;voltage? &amp;nbsp;This is the value predicted by the Freescale battery life calculation&amp;nbsp;tool. A competitor's tool gives AA capacity as 2850mA.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have read the Energizer and Duracell technical manuals and they do not give battery life or capacity for a 1mA constant load.&lt;/P&gt;&lt;P&gt;The charts start at 10mA load.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Oct 2010 20:26:20 GMT</pubDate>
    <dc:creator>Eng8492</dc:creator>
    <dc:date>2010-10-14T20:26:20Z</dc:date>
    <item>
      <title>HCS908LL16/36/64, Battery Capacity, Battery Life Calculation Tool.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS908LL16-36-64-Battery-Capacity-Battery-Life-Calculation-Tool/m-p/155283#M8792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is the authoritative source that gives an AA alkaline cell a capacity of approximately 2800mAh with a 1mA constant load? What did Freescale use for a cutoff&amp;nbsp;voltage? &amp;nbsp;This is the value predicted by the Freescale battery life calculation&amp;nbsp;tool. A competitor's tool gives AA capacity as 2850mA.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have read the Energizer and Duracell technical manuals and they do not give battery life or capacity for a 1mA constant load.&lt;/P&gt;&lt;P&gt;The charts start at 10mA load.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Oct 2010 20:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS908LL16-36-64-Battery-Capacity-Battery-Life-Calculation-Tool/m-p/155283#M8792</guid>
      <dc:creator>Eng8492</dc:creator>
      <dc:date>2010-10-14T20:26:20Z</dc:date>
    </item>
    <item>
      <title>Re: HCS908LL16/36/64, Battery Capacity, Battery Life Calculation Tool.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS908LL16-36-64-Battery-Capacity-Battery-Life-Calculation-Tool/m-p/155284#M8793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For an AA alkaline cell, a load of 10mA would be considered a light load - it is with much heaver loads that the capacity would begin to reduce appreciably.&amp;nbsp; For a primary cell, such as an alkaline type, the unit to unit variation of capacity would probably be subject to a wide tolerance, so the difference between 2800 and 2850 mAh would be negligible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For a 1mA constant current load, I suggest that you use the manufacturer's discharge period for a 10mA load, and simply multiply by 10.&amp;nbsp; The number of hours would then represent the mAh capacity&amp;nbsp;to the particular discharge voltage that you require.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Oct 2010 23:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS908LL16-36-64-Battery-Capacity-Battery-Life-Calculation-Tool/m-p/155284#M8793</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-14T23:15:54Z</dc:date>
    </item>
  </channel>
</rss>