<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックInternal oscillator tolerance after production</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154885#M8757</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;In the manual I found the following sentence: "The internal oscillator circuit is designed for use with no external components to provide a clock source with tolerance less than ±25% untrimmed. An 8-bit trimming register allows adjustment to a tolerance of less than ±5%.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;Now my question:&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;Is the tolerance after production 25% or 5%, what means is the controller after production trimmed or untrimmed?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2007 16:14:51 GMT</pubDate>
    <dc:creator>Hank</dc:creator>
    <dc:date>2007-10-12T16:14:51Z</dc:date>
    <item>
      <title>Internal oscillator tolerance after production</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154885#M8757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;In the manual I found the following sentence: "The internal oscillator circuit is designed for use with no external components to provide a clock source with tolerance less than ±25% untrimmed. An 8-bit trimming register allows adjustment to a tolerance of less than ±5%.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;Now my question:&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 3;"&gt;Is the tolerance after production 25% or 5%, what means is the controller after production trimmed or untrimmed?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2007 16:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154885#M8757</guid>
      <dc:creator>Hank</dc:creator>
      <dc:date>2007-10-12T16:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: Internal oscillator tolerance after production</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154886#M8758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Hank,&lt;BR /&gt;&lt;BR /&gt;Difficult to comment on a book without the reference &lt;SPAN&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;May be you &lt;B&gt;should&lt;/B&gt; read this post: &lt;B&gt;&lt;A class="subj_read" href="http://forums.freescale.com/message?board.id=FORUMUSE&amp;amp;message.id=865" rel="nofollow" target="_blank"&gt;[IMPORTANT] Reminder of Rules to post on technical boards&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/B&gt;You have to see if your provider if he/she is supplying trimmed MCUs or not.&lt;BR /&gt;You can also look at the trim address if the content is $FF or programmed.&lt;BR /&gt;&lt;BR /&gt;When you mass erase the device, you also erase the trim value and have to reprogram it !&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2007 16:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154886#M8758</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-10-12T16:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: Internal oscillator tolerance after production</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154887#M8759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hank,&lt;/DIV&gt;&lt;DIV&gt;I assume that you are looking into the MC68HC908QY4 book or something like it.&lt;/DIV&gt;&lt;DIV&gt;In that book it states what you have read.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The tolerance without any modified OSCTRIM register is 25%, which makes it oscillate at anything from 2.4 MHz to 4 MHz. Untrimmed the value of the OSCTRIM register is 0x80.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the frequency is trimmed, the value will&amp;nbsp;be maximum +/- 5% of, so the frequency will now be 3.04 MHz to 3.36 MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The frequencies are the bus frequencies and are -40 C to + 125, VDD +/- 10%.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;These figures are for the MC68HC908QY/QT.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Note: The OSCTRIM is not automatically loaded. You must take the value, from 0xffc0 and write it into the OSCTRIM register to make it have any effect.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2007 18:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-oscillator-tolerance-after-production/m-p/154887#M8759</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2007-10-12T18:31:43Z</dc:date>
    </item>
  </channel>
</rss>