<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Connecting to PC via USB instead of RS-232</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154883#M8755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Do you mind elaborating it? COTS USB? FTDI?&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Feb 2009 07:28:19 GMT</pubDate>
    <dc:creator>SyaZ</dc:creator>
    <dc:date>2009-02-21T07:28:19Z</dc:date>
    <item>
      <title>Connecting to PC via USB instead of RS-232</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154881#M8753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is pretty general question I think. I have PAN802154 wireless module that I program using USB BDM Multilink. At the end of the day I'd want it connected to PC as coordinator. I noticed I can do this using the RS-232 interface, but using serial port is just inconvenient, and if possible I want to use USB port instead.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any pointers on what can I do? In short I want to be able to do what the BDM Multilink can.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Feb 2009 13:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154881#M8753</guid>
      <dc:creator>SyaZ</dc:creator>
      <dc:date>2009-02-20T13:09:38Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting to PC via USB instead of RS-232</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154882#M8754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The most obvious thing here would be to simply use a COTS USB to Serial converter to achieve this. Another would be to use a chip from FTDI or similar to provide a USB interface on board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Feb 2009 05:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154882#M8754</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-02-21T05:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting to PC via USB instead of RS-232</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154883#M8755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Do you mind elaborating it? COTS USB? FTDI?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Feb 2009 07:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154883#M8755</guid>
      <dc:creator>SyaZ</dc:creator>
      <dc:date>2009-02-21T07:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting to PC via USB instead of RS-232</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154884#M8756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Commercial Off The Shelf i.e. buy one from a shop.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.ftdichip.com/" rel="nofollow" target="_blank"&gt;FTDI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Feb 2009 19:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Connecting-to-PC-via-USB-instead-of-RS-232/m-p/154884#M8756</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-02-21T19:30:30Z</dc:date>
    </item>
  </channel>
</rss>