<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Question on bus frequency for S08QD2 family</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154237#M8673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got a trouble while using S08QD2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used internal clock source, and all ICS settings&amp;nbsp;as default. The bus frequency should be 8M, but I test a timer with 312us, it's actually about 560us.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe it caused by no calibration ICS, am I right? I wonder if any development tool can do calibration for S08 ICS module? I means if possible to do it via BDM using current development tools(like programmer...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2011 09:07:18 GMT</pubDate>
    <dc:creator>eyang</dc:creator>
    <dc:date>2011-07-28T09:07:18Z</dc:date>
    <item>
      <title>Question on bus frequency for S08QD2 family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154237#M8673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got a trouble while using S08QD2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used internal clock source, and all ICS settings&amp;nbsp;as default. The bus frequency should be 8M, but I test a timer with 312us, it's actually about 560us.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe it caused by no calibration ICS, am I right? I wonder if any development tool can do calibration for S08 ICS module? I means if possible to do it via BDM using current development tools(like programmer...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 09:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154237#M8673</guid>
      <dc:creator>eyang</dc:creator>
      <dc:date>2011-07-28T09:07:18Z</dc:date>
    </item>
    <item>
      <title>Re: Question on bus frequency for S08QD2 family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154238#M8674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Recommended USBDM, you can correct ICS, focus is &lt;A href="http://cgi.ebay.com/ws/eBayISAPI.dll?ViewItem&amp;amp;item=120659998381&amp;amp;ssPageName=STRK:MESELX:IT" rel="nofollow" target="_self"&gt;&lt;STRONG&gt;cheap&lt;/STRONG&gt;&lt;/A&gt;, and calibration accuracy is quite high.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 13:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154238#M8674</guid>
      <dc:creator>raining</dc:creator>
      <dc:date>2011-07-28T13:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: Question on bus frequency for S08QD2 family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154239#M8675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You mean USBDM tool can do calibration via PC? Would you please advise me more detail about calibration process.&lt;/P&gt;&lt;P&gt;If I can buy this tools in China?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 16:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154239#M8675</guid>
      <dc:creator>eyang</dc:creator>
      <dc:date>2011-07-28T16:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: Question on bus frequency for S08QD2 family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154240#M8676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can look at the seller's demo movie, which use the standalone programmer, just fill in the required frequency, to download.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 16:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154240#M8676</guid>
      <dc:creator>raining</dc:creator>
      <dc:date>2011-07-28T16:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Question on bus frequency for S08QD2 family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154241#M8677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The maximum&amp;nbsp;untrimmed frequency range for the internal reference is 25-41.66kHz, with a central value of 31.25kHz.&amp;nbsp; This is for an ICSTRM setting of 0x80.&amp;nbsp; The central value corresponds with a &lt;U&gt;maximum&lt;/U&gt; bus frequency of 8MHz.&amp;nbsp; Depending on the ICSC2_BDIV setting, the bus frequency may be &lt;U&gt;reduced&lt;/U&gt; to&amp;nbsp;4MHz, 2MHz or 1MHz nominal.&amp;nbsp; The power-up default setting is for a trimmed bus frequency of 4MHz.&amp;nbsp; You will need to alter the BDIV setting to achieve 8MHz bus frequency.&amp;nbsp; I wonder is this is part of the problem, since the frequency error seems to be too great for the trim setting alone.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check the value within the ICSTRM register.&amp;nbsp; A value of 0x80 represents the power-up default setting.&amp;nbsp; A value of 0xFF would indicate that the setting has been updated from flash memory (address 0xFFAF), to reflect the non-volatile trim setting, but this location has been erased, and&amp;nbsp;no longer holds the factory trim setting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What flash programming tools are you using?&amp;nbsp; CodeWarrior debug mode, in conjunction with P&amp;amp;E USB Multilink BDM interface, certainly is capable calibrating the non-volatile&amp;nbsp;trim settings, at addresses 0xFFAE and 0xFFAF, during the normal programming process.&amp;nbsp; But your code will need to transfer these settings&amp;nbsp;to their respective registers, for trimming to occur.&amp;nbsp; This must be done prior to any&amp;nbsp;change of the BDIV setting, so that the maximum allowable bus frequency&amp;nbsp;is never&amp;nbsp;exceeded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 22:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-on-bus-frequency-for-S08QD2-family/m-p/154241#M8677</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-07-28T22:02:47Z</dc:date>
    </item>
  </channel>
</rss>