<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08GW32 STOP 3 mode in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GW32-STOP-3-mode/m-p/153203#M8520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff, and welcome&amp;nbsp; to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any GPIO pins are not connected to external circuitry, and have not been properly initialised, there will be extra current draw due to inputs that are left floating.&amp;nbsp; After POR, all GPIO pins are inputs.&amp;nbsp; To minimize the current draw, either enable pullups, or alternatively set each&amp;nbsp;unused pin for output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you happen to be using a package with reduced number of&amp;nbsp;pins, for the particular device,&amp;nbsp;the unpinned GPIO must always be initialised in the above manner.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2012 20:52:55 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2012-04-11T20:52:55Z</dc:date>
    <item>
      <title>MC9S08GW32 STOP 3 mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GW32-STOP-3-mode/m-p/153202#M8519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have to try enter STOP 3 mode.&amp;nbsp; The power consumption about 500 uA, but datasheet typical is under 1uA.&lt;/P&gt;&lt;P&gt;How to reduce power consumption? thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SOPT1_STOPE=1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPMSC1_LVDE=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPMSC1_LVDSE=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPMSC2_PPDE=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPMSC2_PPDC=0;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2012 16:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GW32-STOP-3-mode/m-p/153202#M8519</guid>
      <dc:creator>JeffChang</dc:creator>
      <dc:date>2012-04-11T16:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GW32 STOP 3 mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GW32-STOP-3-mode/m-p/153203#M8520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff, and welcome&amp;nbsp; to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any GPIO pins are not connected to external circuitry, and have not been properly initialised, there will be extra current draw due to inputs that are left floating.&amp;nbsp; After POR, all GPIO pins are inputs.&amp;nbsp; To minimize the current draw, either enable pullups, or alternatively set each&amp;nbsp;unused pin for output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you happen to be using a package with reduced number of&amp;nbsp;pins, for the particular device,&amp;nbsp;the unpinned GPIO must always be initialised in the above manner.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2012 20:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GW32-STOP-3-mode/m-p/153203#M8520</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-04-11T20:52:55Z</dc:date>
    </item>
  </channel>
</rss>