<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 64 bit math in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152894#M8434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm attempting to build a DDS setup using A 9S08DN32 , and C in codewarior&amp;nbsp; , I've set up the floating point options with double as IEEE64 ( which I've assumed will allow me to go past a 32 bit limit , and yes I'm a newbie and with no formal C training )&amp;nbsp; Entering large numbers ( above the 32 bit limit gives me a, "illegal number" error , so I can't do the math required to program the DDS !!&lt;/P&gt;&lt;P&gt;I'm taking the basic code outline&amp;nbsp; from an Adruino project which runs without any problems and seems to handle very large numbers without batting an eyelid , however I want to use a Freescale MCU :-)&amp;nbsp; I'm assuming I'm making some obvious mistake , or is codewarrior/ 9s08 MCUs&amp;nbsp; limited compared with the Arduino ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Art&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2012 20:52:03 GMT</pubDate>
    <dc:creator>chop</dc:creator>
    <dc:date>2012-04-10T20:52:03Z</dc:date>
    <item>
      <title>64 bit math</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152894#M8434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm attempting to build a DDS setup using A 9S08DN32 , and C in codewarior&amp;nbsp; , I've set up the floating point options with double as IEEE64 ( which I've assumed will allow me to go past a 32 bit limit , and yes I'm a newbie and with no formal C training )&amp;nbsp; Entering large numbers ( above the 32 bit limit gives me a, "illegal number" error , so I can't do the math required to program the DDS !!&lt;/P&gt;&lt;P&gt;I'm taking the basic code outline&amp;nbsp; from an Adruino project which runs without any problems and seems to handle very large numbers without batting an eyelid , however I want to use a Freescale MCU :-)&amp;nbsp; I'm assuming I'm making some obvious mistake , or is codewarrior/ 9s08 MCUs&amp;nbsp; limited compared with the Arduino ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Art&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2012 20:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152894#M8434</guid>
      <dc:creator>chop</dc:creator>
      <dc:date>2012-04-10T20:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: 64 bit math</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152895#M8435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Try adding decimal point at the end of the number. I mean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;double d;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; d = 5000000000; // &amp;lt;-- illegal error&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; d = 5000000000.0; // &amp;lt;-- OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Integer 5000.. doesn't fit 32bit integer. Since this compiler doesn't support long long int type, probably it complines about all integer constants, which don't fit 32bits. Your Arduino compiler may support long long's.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW Should we guess how do you enter your big number? Is it so hard to copy paste few lines, which trigger compiler error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2012 23:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152895#M8435</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2012-04-10T23:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: 64 bit math</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152896#M8436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That certainly clears up the erroe message , so it's now onward and upward :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks for the reply&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Art&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2012 07:00:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/64-bit-math/m-p/152896#M8436</guid>
      <dc:creator>chop</dc:creator>
      <dc:date>2012-04-12T07:00:39Z</dc:date>
    </item>
  </channel>
</rss>