<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Internal pullup for input capture - 908QY4 and 9S08SH8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152827#M8422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Rob G,&lt;BR /&gt;&lt;BR /&gt;The new SH devices include a port interrupt circuitry which is very similar to the keyboard interrupt module. One of the differences between these two modules is the hability to control the pulling devices independently (no matter they are enabled as port interrupt sources or not).&lt;BR /&gt;&lt;BR /&gt;All you have to do is to enable the respective PTxPE bit and select the desired pulling device through PTxES (1 = pull-up, 0 = pull-down).&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 May 2008 19:24:47 GMT</pubDate>
    <dc:creator>fabio</dc:creator>
    <dc:date>2008-05-05T19:24:47Z</dc:date>
    <item>
      <title>Internal pullup for input capture - 908QY4 and 9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152826#M8421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I understand that the internal pullup resistor is not available when using input capture function on 908QY4A. Does this also apply to the&amp;nbsp;9S08SH8? Should be a simple thing to test but I have not got the hardware yet.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Rob&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Added part numbers to subject.&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-05-04&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:23 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 May 2008 20:08:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152826#M8421</guid>
      <dc:creator>RobG</dc:creator>
      <dc:date>2008-05-04T20:08:42Z</dc:date>
    </item>
    <item>
      <title>Re: Internal pullup for input capture - 908QY4 and 9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152827#M8422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Rob G,&lt;BR /&gt;&lt;BR /&gt;The new SH devices include a port interrupt circuitry which is very similar to the keyboard interrupt module. One of the differences between these two modules is the hability to control the pulling devices independently (no matter they are enabled as port interrupt sources or not).&lt;BR /&gt;&lt;BR /&gt;All you have to do is to enable the respective PTxPE bit and select the desired pulling device through PTxES (1 = pull-up, 0 = pull-down).&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2008 19:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152827#M8422</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-05-05T19:24:47Z</dc:date>
    </item>
    <item>
      <title>Re: Internal pullup for input capture - 908QY4 and 9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152828#M8423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks Fabio, that's a nice improvement over&amp;nbsp;HC08.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Rob&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;b.t.w. Congratulations on your new book. I've had a copy for a couple of weeks. I haven't had time to do more than have a quick look but it looks&amp;nbsp;to be very comprehensive and will be a great resource for beginners and more experienced designers alike.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2008 20:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-pullup-for-input-capture-908QY4-and-9S08SH8/m-p/152828#M8423</guid>
      <dc:creator>RobG</dc:creator>
      <dc:date>2008-05-05T20:49:58Z</dc:date>
    </item>
  </channel>
</rss>