<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152684#M8413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for your suggestion. Could you please tell me what a DVM is?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Apr 2012 06:38:43 GMT</pubDate>
    <dc:creator>apples1234</dc:creator>
    <dc:date>2012-04-17T06:38:43Z</dc:date>
    <item>
      <title>Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152682#M8411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I am a newbie at this. I am trying to interface MMA3204EG dual axis accelerometer with an 8-bit PIC microcontroller. My question is mainly regarding the self-test pin provided in the accelerometer. The datasheet simply states the following:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;When the user applies a logic high input to the selftest&amp;nbsp;pin, a calibrated potential is applied across the self-test&amp;nbsp;plate and the moveable plate. The resulting electrostatic&amp;nbsp;force (Fe = 1/2 AV2/d2) causes the center plate to deflect. The&amp;nbsp;resultant deflection is measured by the accelerometer's&amp;nbsp;control ASIC and a proportional output voltage results.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;My question is, if there is a way to find out a value of this output voltage. When I connect the accelerometer to the microcontroller (as per the specifications mentioned in the datasheet) the values simply fluctuate between 0V and 1V. I do not get any other values. Please help me. Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2012 09:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152682#M8411</guid>
      <dc:creator>apples1234</dc:creator>
      <dc:date>2012-04-10T09:26:27Z</dc:date>
    </item>
    <item>
      <title>Re: Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152683#M8412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My interpretation of the datasheet, with respect to the&amp;nbsp;MMA3204 self test operation, is that a test force equivalent to 12g +/-20 percent is applied to each g-cell.&amp;nbsp; Assuming that Vdd is 5.0 volt, the X-output should step by nominally 0.24 volt, and the Y-output by nominally 0.80 volts, during self test mode.&amp;nbsp; For different Vdd, the output step will be proportional to the Vdd level.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You might check this out, initially using a DVM, prior to attempting analog-to-digital conversion within the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2012 13:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152683#M8412</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-04-10T13:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152684#M8413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for your suggestion. Could you please tell me what a DVM is?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2012 06:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152684#M8413</guid>
      <dc:creator>apples1234</dc:creator>
      <dc:date>2012-04-17T06:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152685#M8414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DVM = digital voltmeter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2012 09:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152685#M8414</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-04-18T09:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problems interfacing MMA3204EG dual axis accelerometer with 8 bit microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152686#M8415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks once again for your suggestion. When I connected the accelerometer to an oscilloscope or a DVM I did get some readings. They were not 2.5V at 0g but they were again in the range of 0V to 1V. This is when I kept the sensor circuit on the board. When I tap it slightly I do get some changes in the voltage upto 3V for both the axes. I guess my question is do you get exact 2.5V values? I have rechecked my circuit and it is according to the scematic given in the data sheet. So I do not know where I am going wrong. Any suggestion would be helpful. Thanks a lot.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2012 03:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-interfacing-MMA3204EG-dual-axis-accelerometer-with-8/m-p/152686#M8415</guid>
      <dc:creator>apples1234</dc:creator>
      <dc:date>2012-04-19T03:43:01Z</dc:date>
    </item>
  </channel>
</rss>