<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 9S08 + digital pot internally? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125911#M835</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Rob:&lt;BR /&gt;&lt;BR /&gt;Are you talking about the impedance to ground? Will a PWM approach work? Will a regular PWM voltage output not work?&lt;BR /&gt;&lt;BR /&gt;I don't know which chip you are using or what you're interfacing to, but if the standard PWM does not get you what you electrically need (varying impedance), you could try modulating the pin impedance in a very crude fashion.&lt;BR /&gt;&lt;BR /&gt;When a pin is an input, it has a very high impedance. When a pin outputs a zero, it has a very low impedance to ground. If the device won't mind the impedance varying between the two extremes in a modulated fashion, you could bit bang the duty cycle.&lt;BR /&gt;&lt;BR /&gt;By putting a zero in the pin's data register and modulating the pin's direction register, you could effect an 'average' impedance over time. You could solicit the help of a timer to bit-bang it, but it may not be very fast.&lt;BR /&gt;&lt;BR /&gt;If you need to vary the impedance to Vcc, simply change the zero in the pin's data register to a one.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 05 Aug 2006 05:04:09 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2006-08-05T05:04:09Z</dc:date>
    <item>
      <title>9S08 + digital pot internally?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125910#M834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Anyone have any digital potentiometer ideas for the 9S08? I've got a very small board with not much room for an external digital pot. Wondered if there's a slick way to vary output impedance on a port pin. Hmmm.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Aug 2006 03:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125910#M834</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2006-08-05T03:09:36Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 + digital pot internally?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125911#M835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Rob:&lt;BR /&gt;&lt;BR /&gt;Are you talking about the impedance to ground? Will a PWM approach work? Will a regular PWM voltage output not work?&lt;BR /&gt;&lt;BR /&gt;I don't know which chip you are using or what you're interfacing to, but if the standard PWM does not get you what you electrically need (varying impedance), you could try modulating the pin impedance in a very crude fashion.&lt;BR /&gt;&lt;BR /&gt;When a pin is an input, it has a very high impedance. When a pin outputs a zero, it has a very low impedance to ground. If the device won't mind the impedance varying between the two extremes in a modulated fashion, you could bit bang the duty cycle.&lt;BR /&gt;&lt;BR /&gt;By putting a zero in the pin's data register and modulating the pin's direction register, you could effect an 'average' impedance over time. You could solicit the help of a timer to bit-bang it, but it may not be very fast.&lt;BR /&gt;&lt;BR /&gt;If you need to vary the impedance to Vcc, simply change the zero in the pin's data register to a one.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Aug 2006 05:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125911#M835</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-08-05T05:04:09Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 + digital pot internally?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125912#M836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I asked the vendor of the chip I'm interfacing to about PWM and they said it was risky (coupling PWM noise into their circuitry). So I guess I'll stick with a tiny 8-pin Microchip DAC.&lt;BR /&gt;&lt;BR /&gt;Thanks for the feedback.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Aug 2006 05:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125912#M836</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2006-08-05T05:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 + digital pot internally?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125913#M837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;why don't you use PWM + a cheap Tiny OpAmp + RC at +INP?&lt;/DIV&gt;&lt;DIV&gt;On the same way I made 4-20mA Current Outputs.&lt;/DIV&gt;&lt;DIV&gt;Truk&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2006 13:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-digital-pot-internally/m-p/125913#M837</guid>
      <dc:creator>Truk</dc:creator>
      <dc:date>2006-09-22T13:16:16Z</dc:date>
    </item>
  </channel>
</rss>