<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TOD and STOP2 on HCS08LL16 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TOD-and-STOP2-on-HCS08LL16/m-p/151936#M8329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying&amp;nbsp;to use the&amp;nbsp;HCS08LL16 to periodically wake from&amp;nbsp;STOP2 using the time-of-day (TOD) module.&amp;nbsp; It appears to sleep for 1 second the first time, but all remaining times only sleeps for about 200uS.&amp;nbsp; Yes, I have port B bit 2 configured as an input and pullup enabled before entering STOP2.&amp;nbsp; Yes, I check for PPDF after reset to determine if reset was due to wake from STOP2.&amp;nbsp;Yes, I'm restoring port config before writing PPDACK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have this implemented and working on the QE128 (using RTC)&amp;nbsp;, but cannot get to work on the LL16 (using TOD).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone out there with an example or tips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Nov 2009 05:23:42 GMT</pubDate>
    <dc:creator>jckruege</dc:creator>
    <dc:date>2009-11-06T05:23:42Z</dc:date>
    <item>
      <title>TOD and STOP2 on HCS08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TOD-and-STOP2-on-HCS08LL16/m-p/151936#M8329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying&amp;nbsp;to use the&amp;nbsp;HCS08LL16 to periodically wake from&amp;nbsp;STOP2 using the time-of-day (TOD) module.&amp;nbsp; It appears to sleep for 1 second the first time, but all remaining times only sleeps for about 200uS.&amp;nbsp; Yes, I have port B bit 2 configured as an input and pullup enabled before entering STOP2.&amp;nbsp; Yes, I check for PPDF after reset to determine if reset was due to wake from STOP2.&amp;nbsp;Yes, I'm restoring port config before writing PPDACK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have this implemented and working on the QE128 (using RTC)&amp;nbsp;, but cannot get to work on the LL16 (using TOD).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone out there with an example or tips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2009 05:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TOD-and-STOP2-on-HCS08LL16/m-p/151936#M8329</guid>
      <dc:creator>jckruege</dc:creator>
      <dc:date>2009-11-06T05:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: TOD and STOP2 on HCS08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TOD-and-STOP2-on-HCS08LL16/m-p/151937#M8330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured it out&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;...I had a damaged&amp;nbsp;board (ESD?)&lt;/P&gt;&lt;P&gt;Tried on another board ... and it works.&lt;/P&gt;&lt;P&gt;Attached is stripped down Codewarrior V6.2 project including source that works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/15236_Project_2.zip" rel="nofollow" target="_self"&gt;Project_2.zip&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-11-08&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;10:26 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Nov 2009 04:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TOD-and-STOP2-on-HCS08LL16/m-p/151937#M8330</guid>
      <dc:creator>jckruege</dc:creator>
      <dc:date>2009-11-07T04:23:30Z</dc:date>
    </item>
  </channel>
</rss>