<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Problems writing FLASh in GT series</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151896#M8328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;I use the P&amp;amp;E Multilink to simulate. But i don't run the code without the BDM. I have to run without it?&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply.&lt;BR /&gt;&lt;BR /&gt;Ariel&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Feb 2009 02:37:24 GMT</pubDate>
    <dc:creator>Armole</dc:creator>
    <dc:date>2009-02-13T02:37:24Z</dc:date>
    <item>
      <title>Problems writing FLASh in GT series</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151894#M8326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to use the bean intFlash from the CW 6.2 and i can't write to flash memory. My code is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;IFsh1_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;IFsh1_SetWordFlash(&amp;amp;add,f);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;add is the 0x8010, and f is a word.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is when i simulate the function SetWordFlash waits for the Flash command to end and it never ends (the COP resets).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;These functions are generated by Processor Experts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please, If anyone can help me&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank You&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 20:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151894#M8326</guid>
      <dc:creator>Armole</dc:creator>
      <dc:date>2009-02-11T20:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problems writing FLASh in GT series</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151895#M8327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, and welcome to the forum.&lt;BR /&gt;&lt;BR /&gt;The full chip simulator within CW does not simulate flash erase and programming processes.&amp;nbsp; You will need to use the actual hardware to test these.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mac&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2009 02:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151895#M8327</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-02-12T02:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Problems writing FLASh in GT series</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151896#M8328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;I use the P&amp;amp;E Multilink to simulate. But i don't run the code without the BDM. I have to run without it?&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply.&lt;BR /&gt;&lt;BR /&gt;Ariel&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2009 02:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-writing-FLASh-in-GT-series/m-p/151896#M8328</guid>
      <dc:creator>Armole</dc:creator>
      <dc:date>2009-02-13T02:37:24Z</dc:date>
    </item>
  </channel>
</rss>