<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: 9S08 with BDM</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125908#M832</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alvin,&lt;/P&gt;&lt;P&gt;I've even tried a 680 ohm pull up...&lt;/P&gt;&lt;P&gt;The 3 100nF&amp;nbsp;capa are soldered closest as possible (less than 2mm, below the 9S08).&lt;/P&gt;&lt;P&gt;Yvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2006 17:21:37 GMT</pubDate>
    <dc:creator>yb</dc:creator>
    <dc:date>2006-02-06T17:21:37Z</dc:date>
    <item>
      <title>9S08 with BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125906#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Since I've used 9S08GB32 and the P&amp;amp;E BDM pod, I've seen the same big problem : in debug mode (with pod plugged and in step by step&amp;nbsp;debug for example), if I light a little lamp near my system, the pod generate a RESET to the 9S08 and come back to the start of the startup.c in STOP mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The problem is seen with any electric consumer (PC monitor, soldering iron...).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Actually, I'm developping a product with a motor control (H bridge with MOSFET) and it's of course impossible to use the debug mode for this reason &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif"&gt;&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I must remove the BDM cable to avoid these reboot.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can I disable the RESET pin on 9S08 ? I have looking for this option, but I'd find nothing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any ideas ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Yvan&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2006 16:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125906#M830</guid>
      <dc:creator>yb</dc:creator>
      <dc:date>2006-02-04T16:02:52Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 with BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125907#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Yvan,&lt;BR /&gt;&lt;BR /&gt;Have you tried with a smaller Pull-up resistor on the Reset PIN like 4.7k ?&lt;BR /&gt;I also think about faster decoupling of the supply pins very close to the MCU to absorb noise in the tracks.&lt;BR /&gt;&lt;BR /&gt;Alvin.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2006 16:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125907#M831</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2006-02-06T16:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 with BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125908#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alvin,&lt;/P&gt;&lt;P&gt;I've even tried a 680 ohm pull up...&lt;/P&gt;&lt;P&gt;The 3 100nF&amp;nbsp;capa are soldered closest as possible (less than 2mm, below the 9S08).&lt;/P&gt;&lt;P&gt;Yvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2006 17:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125908#M832</guid>
      <dc:creator>yb</dc:creator>
      <dc:date>2006-02-06T17:21:37Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08 with BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125909#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;[EnglishAccent Mode]&lt;BR /&gt;Shocking !&lt;BR /&gt;[/EnglishAccent Mode]&lt;/P&gt;&lt;P&gt;Do you only have the reset when the BDM is on, or even when the MCU is alone in its applications.&lt;/P&gt;&lt;P&gt;If it's the former, the interface may generate a reset when it receives the noise. Grounded kitchen foil around the purple box ? I know it looks like cooking... but it should improve EMI immunity of the BDM interface.&lt;/P&gt;&lt;P&gt;If the latter, can you capture/observe&amp;nbsp;spikes on any particular pin ? This would allow to isolate&amp;nbsp;source and then treat it...&lt;/P&gt;&lt;P&gt;You probably have better experience than me on this, but a new light can always be beneficial &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;.&lt;/P&gt;&lt;P&gt;Alvin.&lt;/P&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2006 18:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08-with-BDM/m-p/125909#M833</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2006-02-06T18:31:52Z</dc:date>
    </item>
  </channel>
</rss>