<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: CW debugger not loading source code</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151219#M8201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exactly the same problem, same CodeWarrior version 5.9.0.&lt;/P&gt;&lt;P&gt;Also working w assembler absolute code.&lt;/P&gt;&lt;P&gt;On a S12E64 mpu though but that should not matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I copy back all files from my safetybackup, it works nicely.&lt;/P&gt;&lt;P&gt;The sourcecode appears nicely in the debugger.&lt;/P&gt;&lt;P&gt;But as soon as I want to change the sourcecode to another file&lt;BR /&gt;(by "remove file from project" and "add file to project")&lt;/P&gt;&lt;P&gt;(as I have done hundred of times before, and it still works on other projects in subdirectories parallell to this one)&lt;/P&gt;&lt;P&gt;then the "Enable debugger for target "Standard" window appear.&lt;/P&gt;&lt;P&gt;No matter what I select Yes/No/Cancel the debugger starts with sourcecode missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLEASE SOMEONE HELP !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I dont want to have to create a complete new project everytime I am updating/changing back a version of my code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jan 2015 16:18:02 GMT</pubDate>
    <dc:creator>GsFilm</dc:creator>
    <dc:date>2015-01-22T16:18:02Z</dc:date>
    <item>
      <title>CW debugger not loading source code</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151216#M8198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have made a new project with CodeWarrior and copied into it an existing code file, as I have done OK in the past.&lt;/P&gt;&lt;P&gt;(machine code only, absolute assembly)&lt;/P&gt;&lt;P&gt;Two problems occur, (which may be related) , when I start a Debug session:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) On debug startup, a Yes/No window shows which states:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;'Enable Debugger for Target 'standard'. The debugger requires certain target settings in order to function correctly. Do you &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; want &amp;nbsp;CW to configure these settings automatically for target 'standard' ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) the source code does not load into the debugger....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas how to fix these problems?&lt;/P&gt;&lt;P&gt;CW v5.9.0, Debugger v6.1, &amp;nbsp;'08JM60 cpu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2011 14:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151216#M8198</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2011-07-19T14:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: CW debugger not loading source code</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151217#M8199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had this happen recently,&amp;nbsp; not sure why.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I managed to make it work by forcing the debugger to load the source.&amp;nbsp; There are menu items for this,&amp;nbsp; and I don't recall exactly what I had to do.&amp;nbsp; I think it was the multilinkcyclonepro menu,&amp;nbsp; load,&amp;nbsp; and check a bunch of checkboxes near the bottom.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think I was working with the CFV1 beta version of the AN2295 bootloader.&amp;nbsp; But its 1:30 AM here,&amp;nbsp; so my memory may be faulty...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2011 12:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151217#M8199</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-08-08T12:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: CW debugger not loading source code</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151218#M8200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have fixed the problem by creating a new project.&lt;/P&gt;&lt;P&gt;It seems the compiler/debugger &amp;nbsp;doesn't like the project to be nested into too many subdirectories....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2011 12:35:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151218#M8200</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2011-08-08T12:35:34Z</dc:date>
    </item>
    <item>
      <title>Re: CW debugger not loading source code</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151219#M8201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exactly the same problem, same CodeWarrior version 5.9.0.&lt;/P&gt;&lt;P&gt;Also working w assembler absolute code.&lt;/P&gt;&lt;P&gt;On a S12E64 mpu though but that should not matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I copy back all files from my safetybackup, it works nicely.&lt;/P&gt;&lt;P&gt;The sourcecode appears nicely in the debugger.&lt;/P&gt;&lt;P&gt;But as soon as I want to change the sourcecode to another file&lt;BR /&gt;(by "remove file from project" and "add file to project")&lt;/P&gt;&lt;P&gt;(as I have done hundred of times before, and it still works on other projects in subdirectories parallell to this one)&lt;/P&gt;&lt;P&gt;then the "Enable debugger for target "Standard" window appear.&lt;/P&gt;&lt;P&gt;No matter what I select Yes/No/Cancel the debugger starts with sourcecode missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLEASE SOMEONE HELP !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I dont want to have to create a complete new project everytime I am updating/changing back a version of my code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 16:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CW-debugger-not-loading-source-code/m-p/151219#M8201</guid>
      <dc:creator>GsFilm</dc:creator>
      <dc:date>2015-01-22T16:18:02Z</dc:date>
    </item>
  </channel>
</rss>