<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: 908JK3 - clearing TOF bit.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151053#M8144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Aha!&lt;/P&gt;&lt;P&gt;I was imagining you had to read the whole byte.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, peg.&amp;nbsp; &lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Sep 2010 10:03:41 GMT</pubDate>
    <dc:creator>JimDandy</dc:creator>
    <dc:date>2010-09-28T10:03:41Z</dc:date>
    <item>
      <title>908JK3 - clearing TOF bit.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151051#M8142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the manual:&lt;/P&gt;&lt;P&gt;"Clear TOF by reading the TIM status and control register when TOF is set and then writing a zero to TOF."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now if the timer has overflowed I have no use for the data it now contains, so to clear the TOF bit do I still have to do a dummy read of TSC and then clear the TOF bit, or can I just clear the TOF bit and be done with it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Sep 2010 17:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151051#M8142</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2010-09-25T17:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: 908JK3 - clearing TOF bit.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151052#M8143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes you must still do the read.&lt;/P&gt;&lt;P&gt;However if you use BCLR this is a read-modify-write and so does this in one instruction.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Sep 2010 04:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151052#M8143</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-28T04:09:29Z</dc:date>
    </item>
    <item>
      <title>Re: 908JK3 - clearing TOF bit.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151053#M8144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Aha!&lt;/P&gt;&lt;P&gt;I was imagining you had to read the whole byte.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, peg.&amp;nbsp; &lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Sep 2010 10:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151053#M8144</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2010-09-28T10:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: 908JK3 - clearing TOF bit.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151054#M8145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And you make CPU reading whole byte. Doing BSET/BCLR CPU still is reading and writing whole memory bytes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Sep 2010 11:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908JK3-clearing-TOF-bit/m-p/151054#M8145</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-09-28T11:05:14Z</dc:date>
    </item>
  </channel>
</rss>