<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SG8 continuous reset in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150119#M8036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I facing a strange issue of continuous reset on my S9S08SG8 board. The SG8 seems to be resetting continously as the scope connected to reset pin shows a square wave of about 25Khz. To isolate the problem I connected only VDD and GND with a 10K pull up to RST. I can still see a 25Khz squre wave on RST.&lt;/P&gt;&lt;P&gt;If I pull up the BKGD/MS pin while booting, RST shows steady 5 V. P&amp;amp;E is unable to program the IC.&lt;/P&gt;&lt;P&gt;Am I missing something ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Pramod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2009 23:06:04 GMT</pubDate>
    <dc:creator>layman</dc:creator>
    <dc:date>2009-10-28T23:06:04Z</dc:date>
    <item>
      <title>SG8 continuous reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150119#M8036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I facing a strange issue of continuous reset on my S9S08SG8 board. The SG8 seems to be resetting continously as the scope connected to reset pin shows a square wave of about 25Khz. To isolate the problem I connected only VDD and GND with a 10K pull up to RST. I can still see a 25Khz squre wave on RST.&lt;/P&gt;&lt;P&gt;If I pull up the BKGD/MS pin while booting, RST shows steady 5 V. P&amp;amp;E is unable to program the IC.&lt;/P&gt;&lt;P&gt;Am I missing something ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Pramod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2009 23:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150119#M8036</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-28T23:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: SG8 continuous reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150120#M8037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;Correction : It should be&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;EM&gt;If I &lt;STRONG&gt;pull&amp;nbsp;down&lt;/STRONG&gt; the BKGD/MS pin while booting, RST shows steady 5 V. P&amp;amp;E is unable to program the IC.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;instead of&lt;/P&gt;&lt;P&gt;&lt;EM&gt;If I &lt;STRONG&gt;pull up&lt;/STRONG&gt; the BKGD/MS pin while booting, RST shows steady 5 V. P&amp;amp;E is unable to program the IC.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Pramod&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2009 11:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150120#M8037</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-29T11:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: SG8 continuous reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150121#M8038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Pramad,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The symptoms you describe are usually caused by a COP timeout or Illegal instruction reset.&amp;nbsp; Judging by the frequency I suspect the latter.&amp;nbsp; Holding BKGD low during power-on causes the device to enter BDM mode disabling the COP and instruction execution.&amp;nbsp; This can occur if the chip is blank or programmed incorrectly.&amp;nbsp; Once programmed it usually isn't a problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would expect that the P&amp;amp;E BDM would be able to&amp;nbsp; to do the same thing (i.e. hold BKGD low) while prompting you to cycle the target power.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the P&amp;amp;E BDM work with other chips?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so try the following sequence:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hold BKGD low while powering on (use a 100R resistor if it works to avoid damaging the BDM).&lt;/P&gt;&lt;P&gt;Connect the P&amp;amp;E BDM.&lt;/P&gt;&lt;P&gt;Release the BKGD pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See if the BDM can connect now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-29&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:11 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2009 13:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150121#M8038</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-10-29T13:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: SG8 continuous reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150122#M8039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks PGO !!!&lt;/P&gt;&lt;P&gt;Holding the BKGD low manually seems to solve the problem. I expected the P&amp;amp;E to take care of this but for some reason it doesnt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2009 19:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SG8-continuous-reset/m-p/150122#M8039</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-29T19:05:40Z</dc:date>
    </item>
  </channel>
</rss>