<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Windows 7 &amp; SimpleUSB in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Windows-7-SimpleUSB/m-p/150010#M8022</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I realize there are several topics in this forum regarding using SimpleUSB.dll with Windows 7, however, I have come across a problem that I have not seen addressed as of yet.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have developed a simple C# gui application for a demoJM board and used simpleUSB to interface with the board (following the tutorial posted on your website).&amp;nbsp; The problem is that the program runs perfectly fine on any XP machine but when running the program on a Windows 7 x86 machine, communication between the program and the board eventually dies.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice regarding this issue would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2011 00:59:34 GMT</pubDate>
    <dc:creator>jpapaTN</dc:creator>
    <dc:date>2011-07-15T00:59:34Z</dc:date>
    <item>
      <title>Windows 7 &amp; SimpleUSB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Windows-7-SimpleUSB/m-p/150010#M8022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I realize there are several topics in this forum regarding using SimpleUSB.dll with Windows 7, however, I have come across a problem that I have not seen addressed as of yet.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have developed a simple C# gui application for a demoJM board and used simpleUSB to interface with the board (following the tutorial posted on your website).&amp;nbsp; The problem is that the program runs perfectly fine on any XP machine but when running the program on a Windows 7 x86 machine, communication between the program and the board eventually dies.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice regarding this issue would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2011 00:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Windows-7-SimpleUSB/m-p/150010#M8022</guid>
      <dc:creator>jpapaTN</dc:creator>
      <dc:date>2011-07-15T00:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 &amp; SimpleUSB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Windows-7-SimpleUSB/m-p/150011#M8023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A __default_attr="80364" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/80364" jivemacro="thread" title="https://community.freescale.com/thread/80364"&gt;https://community.freescale.com/thread/80364&lt;/A&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2011 23:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Windows-7-SimpleUSB/m-p/150011#M8023</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2011-08-26T23:22:04Z</dc:date>
    </item>
  </channel>
</rss>