<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: L1822 Error in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149666#M7990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank Jim and Kev, it worked&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jul 2011 23:28:08 GMT</pubDate>
    <dc:creator>Idontunderstand</dc:creator>
    <dc:date>2011-07-14T23:28:08Z</dc:date>
    <item>
      <title>L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149661#M7985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dear;&lt;/P&gt;&lt;P&gt;I am using CSMB12-C128 using codewarrior.&lt;/P&gt;&lt;P&gt;I formated my computer so I forced to install codewarrior again (I installed version 5.9.0&amp;nbsp; for HCS12 series). Now, I got an error on the code which worked fine before.&lt;/P&gt;&lt;P&gt;The errors are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FMUL in file C:\Documents and Settings\Saba\Desktop\FlexSensor_Hand\Project\Project_Data\Standard\ObjectCode\main.c.o&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; is undefined&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FSUB in file C:\Documents and Settings\Saba\Desktop\FlexSensor_Hand\Project\Project_Data\Standard\ObjectCode\main.c.o&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; is undefined&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FADD in file C:\Documents and Settings\Saba\Desktop\FlexSensor_Hand\Project\Project_Data\Standard\ObjectCode\main.c.o&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; is undefined&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FUTRUNC in file C:\Documents and Settings\Saba\Desktop\FlexSensor_Hand\Project\Project_Data\Standard\ObjectCode\main.c.o&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; is undefined&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FSTRUNC in file C:\Documents and Settings\Saba\Desktop\FlexSensor_Hand\Project\Project_Data\Standard\ObjectCode\main.c.o&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; is undefined&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Link Error&amp;nbsp;&amp;nbsp; : Link failed&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;I couldn't find the reason by searching he semiliar questions in the forum. I appreciate any help..&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 09:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149661#M7985</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-14T09:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149662#M7986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You missing the floating point library.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 09:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149662#M7986</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-07-14T09:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149663#M7987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jim.&lt;/P&gt;&lt;P&gt;Could tell me how should I add it, where is that library located?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 12:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149663#M7987</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-14T12:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149664#M7988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When creating new project, you should tell project wizard that you want floating point. Wizard then adds required library. What library to add is specified in &amp;lt;CW intall folder&amp;gt;\lib\hc12c\readme.txt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW, S12 is 16-bit MCU. Please use right forum next time. Keep in mind that there are dedicated Codewarrior forums. This thread should be in "Codewarrior 8- adn 16- bit"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 13:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149664#M7988</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-07-14T13:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149665#M7989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kef gave the answer I would have, because I have not used that version of CW in quite some time. If you fish around in the project settings, there may be something there, other than that you will have to regenerate the project and specifiy floating point.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 19:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149665#M7989</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-07-14T19:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: L1822 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149666#M7990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank Jim and Kev, it worked&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 23:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1822-Error/m-p/149666#M7990</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-14T23:28:08Z</dc:date>
    </item>
  </channel>
</rss>