<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MMA7361L question</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149312#M7858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora, Greg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Virtually all analogue outputs are affected by the load imposed on them by the following stage.&lt;/P&gt;&lt;P&gt;So they are specified with a minimum loading that can be applied and still remain with in specification.&lt;/P&gt;&lt;P&gt;If the input impedance of whatever you are trying to connect to this output is less than the specified amount then interposing a resistor does not really help.&lt;/P&gt;&lt;P&gt;This will just move the source of the error from within the device to the resistor.&lt;/P&gt;&lt;P&gt;If you really must use a connected device that has a below spec. input impedance than usually you would need to interpose an op-amp or the like to handle the impedance mismatch. A simple voltage follower (gain=1) setup will usually suffice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Sep 2010 05:51:08 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2010-09-22T05:51:08Z</dc:date>
    <item>
      <title>MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149311#M7857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings to everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and sorry for posting an accelerometer related question here but there seems to be no dedicated subforum for these tiny devices. &amp;nbsp;Please help me understanding this in the &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Ffiles%2Fsensors%2Fdoc%2Fdata_sheet%2FMMA7361L.pdf" rel="nofollow" target="_blank"&gt;datasheet, page 5&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"10 MΩ or higher is recommended on XOUT, YOUT and&lt;BR /&gt;ZOUT to prevent loss due to the voltage divider&lt;BR /&gt;relationship between the internal 32 kΩ resistor and&lt;BR /&gt;the measurement input impedance."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does it mean that I need to connect &amp;nbsp;1MOhm resistors in series with each output of the accelerometer?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Sep 2010 05:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149311#M7857</guid>
      <dc:creator>justgreg</dc:creator>
      <dc:date>2010-09-22T05:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149312#M7858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora, Greg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Virtually all analogue outputs are affected by the load imposed on them by the following stage.&lt;/P&gt;&lt;P&gt;So they are specified with a minimum loading that can be applied and still remain with in specification.&lt;/P&gt;&lt;P&gt;If the input impedance of whatever you are trying to connect to this output is less than the specified amount then interposing a resistor does not really help.&lt;/P&gt;&lt;P&gt;This will just move the source of the error from within the device to the resistor.&lt;/P&gt;&lt;P&gt;If you really must use a connected device that has a below spec. input impedance than usually you would need to interpose an op-amp or the like to handle the impedance mismatch. A simple voltage follower (gain=1) setup will usually suffice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Sep 2010 05:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149312#M7858</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-22T05:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149313#M7859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PEG is 100% correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I now use an op-amp configured as a voltage follower to buffer all ADC inputs.&amp;nbsp; Most ADC's are very ugly impedance wise and not only are they usually low impedance, they modulate the impedance making for sometimes erroneous readings.&amp;nbsp; It is one thing to use an ADC to measure a pot which is very steady state and quite another thing to use an ADC to measure the output of a dynamic circuit with a relatively high (&amp;gt; 1Kohm) output impedance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I recommend you always use an op-amp buffer for development until you experimentally verify it is unnecessary for your application.&amp;nbsp; Op-Amps are inexpensive compared to engineering time unless you are high volume and then you can afford to spend engineering dollars to remove components.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good Luck,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Sep 2010 21:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149313#M7859</guid>
      <dc:creator>PeterHouse</dc:creator>
      <dc:date>2010-09-22T21:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149314#M7860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Peg!&amp;nbsp; I would like to connect the X,Y,Z outputs of the accelerometer to an AD7799 3 ch A/D converter. I went through the AD7799 specs but there are no input impedance values listed. However, the A/D can be internally configured to enable its on-chip input buffers this is what you suggested and what I'm going to use. Thanks again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Sep 2010 01:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149314#M7860</guid>
      <dc:creator>justgreg</dc:creator>
      <dc:date>2010-09-23T01:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149315#M7861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Agree, I usually have a couple of MCP601s around. I was just not sure in my reading - English is not my mother tongue, you probably noticed &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Sep 2010 01:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149315#M7861</guid>
      <dc:creator>justgreg</dc:creator>
      <dc:date>2010-09-23T01:20:55Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7361L question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149316#M7862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Greg,&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;justgreg wrote:&lt;BR /&gt;&lt;P&gt;I would like to connect the X,Y,Z outputs of the accelerometer to an AD7799 3 ch A/D converter. I went through the AD7799 specs but there are no input impedance values listed. However, the A/D can be internally configured to enable its on-chip input buffers this is what you suggested and what I'm going to use. Thanks again,&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The input current specification for the AD7799 suggests that the input resistance to the converter would be in the vicinity of 2.5 Mohm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However I do question the choice of a 24-bit A-to-D converter for use with the accelerometer device, which has&amp;nbsp;a non-linearity of up to 1 percent.&amp;nbsp; This would seem to be a significant "over kill".&amp;nbsp; A resolution of 10 or 12 bits should be adequate.&amp;nbsp; Since there is an internal sampling arrangement within the accelerometer, the outputs will likely have some sampling noise present, further limiting actual resolution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Depending on your application, a maximum A-to-D sampling rate of 470Hz may also be a limiting factor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Oct 2010 09:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7361L-question/m-p/149316#M7862</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-05T09:35:06Z</dc:date>
    </item>
  </channel>
</rss>