<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Frequency Problem - ICS in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Frequency-Problem-ICS/m-p/149156#M7848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can add that once I debbug the project the ICS registers has these values:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ICSC1 = 0x04&lt;/P&gt;&lt;P&gt;ICSC2 = 0x40&lt;/P&gt;&lt;P&gt;ICSTRM = 0xa5&lt;/P&gt;&lt;P&gt;ICSSC = 0x11&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Mar 2012 07:17:18 GMT</pubDate>
    <dc:creator>CarlosCba</dc:creator>
    <dc:date>2012-03-28T07:17:18Z</dc:date>
    <item>
      <title>Frequency Problem - ICS</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Frequency-Problem-ICS/m-p/149155#M7847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was trying to configure the SCI module of my MC9S08SH and I make a very simple code, it just send a "2" by the TxD.&lt;/P&gt;&lt;P&gt;But it never works, so I start to look for the problem in RS232 circuit and in the PC but nothing. So I doubt about the frequency clock, because I supposed that it was 8 Mhz just because I read an example, but reading different articles I discover the ICS register.And now I am thinking that the problem is there, because the configured frequency is not the one I thought.&lt;/P&gt;&lt;P&gt;My debbuger is an OSBDM and CW 10.1. I read that "during the flash programming process, the internal reference needs to be calibrated for a frequency of 39.0625 kHz. &amp;nbsp;This is the "non-volatile (NV) trim", and is programmed to a specific flash memory location"&lt;/P&gt;&lt;P&gt;A really do not know how to calibrate the bus frequency, Which register I must load to have a 39.0625kHz frequency? How to do it?&lt;/P&gt;&lt;P&gt;If somebody could help me to know which is the bus frequency , and how it works and can be calibrated I will be very grateful.&lt;/P&gt;&lt;P&gt;Thanks very much for your help in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PD: Sorry for my english is not my native language.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2012 08:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Frequency-Problem-ICS/m-p/149155#M7847</guid>
      <dc:creator>CarlosCba</dc:creator>
      <dc:date>2012-03-27T08:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: Frequency Problem - ICS</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Frequency-Problem-ICS/m-p/149156#M7848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can add that once I debbug the project the ICS registers has these values:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ICSC1 = 0x04&lt;/P&gt;&lt;P&gt;ICSC2 = 0x40&lt;/P&gt;&lt;P&gt;ICSTRM = 0xa5&lt;/P&gt;&lt;P&gt;ICSSC = 0x11&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2012 07:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Frequency-Problem-ICS/m-p/149156#M7848</guid>
      <dc:creator>CarlosCba</dc:creator>
      <dc:date>2012-03-28T07:17:18Z</dc:date>
    </item>
  </channel>
</rss>