<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC1321 Evaluation Board (NCB) usage</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149140#M7844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have been using the sample accelerometer program for SMAC, generated through the beekit tool on the two SRBs that I have received with the kit. I was wondering if I can use the NCB (I can see that the beekit application has the option to generate the code for NCB) where the NCB will act as a PC_Radio and both SRBs will act as&amp;nbsp; acceleremeters and will send the data to the NCB which will inturn send the data over to the PC over the serial port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I could use the two SRBs one acting as the PC_Radio and the other as an accelerometer. Can this same scenario be repeated by replacing the SRB that is connected to the PC by a NCB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking at the code generated for the NCB, I see that it will transfer the data to the PC on the USB port. Can we have it on the serial port too?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does the SMAC allow two SRBs to talk to the NCB at the same time?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Saurabh.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Apr 2008 12:46:52 GMT</pubDate>
    <dc:creator>saurabh</dc:creator>
    <dc:date>2008-04-22T12:46:52Z</dc:date>
    <item>
      <title>MC1321 Evaluation Board (NCB) usage</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149140#M7844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have been using the sample accelerometer program for SMAC, generated through the beekit tool on the two SRBs that I have received with the kit. I was wondering if I can use the NCB (I can see that the beekit application has the option to generate the code for NCB) where the NCB will act as a PC_Radio and both SRBs will act as&amp;nbsp; acceleremeters and will send the data to the NCB which will inturn send the data over to the PC over the serial port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I could use the two SRBs one acting as the PC_Radio and the other as an accelerometer. Can this same scenario be repeated by replacing the SRB that is connected to the PC by a NCB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking at the code generated for the NCB, I see that it will transfer the data to the PC on the USB port. Can we have it on the serial port too?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does the SMAC allow two SRBs to talk to the NCB at the same time?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Saurabh.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Apr 2008 12:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149140#M7844</guid>
      <dc:creator>saurabh</dc:creator>
      <dc:date>2008-04-22T12:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: MC1321 Evaluation Board (NCB) usage</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149141#M7845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hello Saurabh,&lt;BR /&gt;&lt;BR /&gt;You can replace the SRB board that is connected to PC with a NCB board. You have the possibility to select on with port (RS232 or USB) to connect the NCB board to PC, from BeeKit, when you generate the project for SMAC, from Platform -&amp;gt; board_config.h -&amp;gt; Default SCI port: SCI1 = UART on RS232 Connector or&lt;BR /&gt;SCI2 = UART on USB Connector. Also, SMAC allow two SRBs to talk to the NCB at the same time, but you should write your own code for this.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Adrian&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Apr 2008 16:33:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149141#M7845</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2008-04-22T16:33:04Z</dc:date>
    </item>
    <item>
      <title>Re: MC1321 Evaluation Board (NCB) usage</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149142#M7846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the help. It did solve my problem.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2008 11:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321-Evaluation-Board-NCB-usage/m-p/149142#M7846</guid>
      <dc:creator>saurabh</dc:creator>
      <dc:date>2008-04-29T11:14:28Z</dc:date>
    </item>
  </channel>
</rss>