<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: S08QG External Oscillator Connection?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QG-External-Oscillator-Connection/m-p/148526#M7722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EREFS in ICSC2 decides whether the oscillator or an external clock is used. &amp;nbsp; In the latter case, the XTAL pin is freed for I/O use.&amp;nbsp; Use EREFS=0 (reset default) for external clock.&amp;nbsp;&amp;nbsp; But you must also set IREFS=0 in ICSC1 to switch from internal to external clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Oct 2009 02:48:28 GMT</pubDate>
    <dc:creator>tonyp</dc:creator>
    <dc:date>2009-10-23T02:48:28Z</dc:date>
    <item>
      <title>S08QG External Oscillator Connection?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QG-External-Oscillator-Connection/m-p/148525#M7721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;New project, internal clock was fine for my previous first with project with the part, and I am at the pin assignment and product functionality part of the next.&amp;nbsp; I may want to time an event with more precision than the internal clock.&amp;nbsp; With an external crystal taking up two pins, I have none left for the timing function or have to give up some other function.&amp;nbsp; Can I just use one of those oscillator modules?&amp;nbsp; EXTAL seem right for the connection but I have not yet located a clear cut statement in the data sheet to that effect.&amp;nbsp; Cost is not much of an issue.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Oct 2009 01:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QG-External-Oscillator-Connection/m-p/148525#M7721</guid>
      <dc:creator>DSbob</dc:creator>
      <dc:date>2009-10-23T01:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: S08QG External Oscillator Connection?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QG-External-Oscillator-Connection/m-p/148526#M7722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EREFS in ICSC2 decides whether the oscillator or an external clock is used. &amp;nbsp; In the latter case, the XTAL pin is freed for I/O use.&amp;nbsp; Use EREFS=0 (reset default) for external clock.&amp;nbsp;&amp;nbsp; But you must also set IREFS=0 in ICSC1 to switch from internal to external clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Oct 2009 02:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QG-External-Oscillator-Connection/m-p/148526#M7722</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2009-10-23T02:48:28Z</dc:date>
    </item>
  </channel>
</rss>