<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HCS08DZ60 PIN bit in SRS Register is not set in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148462#M7708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Probem the SRS registers.&lt;/P&gt;&lt;P&gt;the Definiton of the SRS is&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;bit7&amp;nbsp;&amp;nbsp; bit6 &amp;nbsp; bit5 &amp;nbsp; bit4 &amp;nbsp; bit3 &amp;nbsp; bit2&amp;nbsp; bit1 &amp;nbsp; bit0&lt;/P&gt;&lt;P&gt;POR &amp;nbsp; PIN &amp;nbsp; COP &amp;nbsp; ILOP&amp;nbsp; ILAD&amp;nbsp; LOC&amp;nbsp; LVD &amp;nbsp;&amp;nbsp; --&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;I generate a Reset signal on the Reset Pin of the µC and the µC will reset itself. After that I read the SRS Register somewhere in the code, I get a value of sometimes 0x40 (PIN ist set), and sometimes 0x2(LVD is set).&amp;nbsp; Wha I expect is that the bit6 "PIN" should always be set. I can't understand why the LVD bit is set and if it is set why the bit "PIN" is not set?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Oct 2009 21:58:45 GMT</pubDate>
    <dc:creator>wander_zhang</dc:creator>
    <dc:date>2009-10-22T21:58:45Z</dc:date>
    <item>
      <title>HCS08DZ60 PIN bit in SRS Register is not set</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148462#M7708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Probem the SRS registers.&lt;/P&gt;&lt;P&gt;the Definiton of the SRS is&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;bit7&amp;nbsp;&amp;nbsp; bit6 &amp;nbsp; bit5 &amp;nbsp; bit4 &amp;nbsp; bit3 &amp;nbsp; bit2&amp;nbsp; bit1 &amp;nbsp; bit0&lt;/P&gt;&lt;P&gt;POR &amp;nbsp; PIN &amp;nbsp; COP &amp;nbsp; ILOP&amp;nbsp; ILAD&amp;nbsp; LOC&amp;nbsp; LVD &amp;nbsp;&amp;nbsp; --&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;I generate a Reset signal on the Reset Pin of the µC and the µC will reset itself. After that I read the SRS Register somewhere in the code, I get a value of sometimes 0x40 (PIN ist set), and sometimes 0x2(LVD is set).&amp;nbsp; Wha I expect is that the bit6 "PIN" should always be set. I can't understand why the LVD bit is set and if it is set why the bit "PIN" is not set?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 21:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148462#M7708</guid>
      <dc:creator>wander_zhang</dc:creator>
      <dc:date>2009-10-22T21:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08DZ60 PIN bit in SRS Register is not set</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148463#M7709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem.&amp;nbsp; Did you solve this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Dec 2010 09:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148463#M7709</guid>
      <dc:creator>Nik</dc:creator>
      <dc:date>2010-12-08T09:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08DZ60 PIN bit in SRS Register is not set</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148464#M7710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It was a long time ago. But I dont think the problem is resolved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Chunyu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Dec 2010 16:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60-PIN-bit-in-SRS-Register-is-not-set/m-p/148464#M7710</guid>
      <dc:creator>wander_zhang</dc:creator>
      <dc:date>2010-12-08T16:04:47Z</dc:date>
    </item>
  </channel>
</rss>