<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LCD drive problem in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/147999#M7595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Try to put some external pullups on the lines. Bye Jack&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Feb 2009 21:12:52 GMT</pubDate>
    <dc:creator>jag</dc:creator>
    <dc:date>2009-02-02T21:12:52Z</dc:date>
    <item>
      <title>LCD drive problem - MC09S08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/147998#M7594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LCD drive problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to drive a 8x24 LCD drive. LCD voltage is 3V and f = 51 Hz. via MC09S08LL16 microcontrller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Problem;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I set more than 3 segment on the same Frontplane the other segments are also appear but they are weak.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I set only one segment this segment is also weak.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1 to 3 segment is working fine. The position of the segment doesnt care, but they must be on the same FP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope someone can help me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2009-02-02&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;06:24 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2009 00:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/147998#M7594</guid>
      <dc:creator>Javercis</dc:creator>
      <dc:date>2009-02-02T00:57:03Z</dc:date>
    </item>
    <item>
      <title>Re: LCD drive problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/147999#M7595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Try to put some external pullups on the lines. Bye Jack&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2009 21:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/147999#M7595</guid>
      <dc:creator>jag</dc:creator>
      <dc:date>2009-02-02T21:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: LCD drive problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/148000#M7596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thanks for advise,&lt;BR /&gt;&lt;BR /&gt;I change the configuration from Charge Pump enable to resistor devider enable and the problem is gone.&lt;BR /&gt;&lt;BR /&gt;I hope the solution is not temporay..&lt;BR /&gt;Thanks ain for your attention...&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2009 04:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LCD-drive-problem-MC09S08LL16/m-p/148000#M7596</guid>
      <dc:creator>Javercis</dc:creator>
      <dc:date>2009-02-04T04:59:58Z</dc:date>
    </item>
  </channel>
</rss>