<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: JM60 @ 3.3V?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147509#M7480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Don! Good idea on the KBI, too.&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Oct 2009 20:40:25 GMT</pubDate>
    <dc:creator>ballen</dc:creator>
    <dc:date>2009-10-19T20:40:25Z</dc:date>
    <item>
      <title>JM60 @ 3.3V?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147507#M7478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm thinking of using the JM60&amp;nbsp;at 3.3V. The data sheet&amp;nbsp;gives&amp;nbsp;specs at 3V, so&amp;nbsp;it must be&amp;nbsp;ok, but I'm wondering why Vcc(typ) is listed at 5V. Are&amp;nbsp;there&amp;nbsp;any issues that aren't obvious? The only one that jumps out is the USB voltage regulator Vin(min) of 3.9V, which&amp;nbsp;could easily be handled with a seperate supply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone tried this? Anything unusual I should be aware of...?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2009 22:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147507#M7478</guid>
      <dc:creator>ballen</dc:creator>
      <dc:date>2009-10-16T22:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 @ 3.3V?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147508#M7479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The JM60 works at full speed @ 3v3 OK. No catches except&lt;/P&gt;&lt;P&gt;for the USB supply as you note. (Disable the on board regulator and feed in&lt;/P&gt;&lt;P&gt;3v3 through a regulator from the USB Volt feed).&lt;/P&gt;&lt;P&gt;I connect port G0 (the next pin along) to the USB power pin, so I get a keyboard interrupt&lt;/P&gt;&lt;P&gt;when the USB is plugged in.&lt;/P&gt;&lt;P&gt;Note also for USB operation you need an external xtal 1 to 4 mhz.&lt;/P&gt;&lt;P&gt;And don't forget to set the Low Volt Detector to the correct trip voltage!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Oct 2009 03:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147508#M7479</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2009-10-17T03:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 @ 3.3V?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147509#M7480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Don! Good idea on the KBI, too.&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2009 20:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-3-3V/m-p/147509#M7480</guid>
      <dc:creator>ballen</dc:creator>
      <dc:date>2009-10-19T20:40:25Z</dc:date>
    </item>
  </channel>
</rss>