<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: IO current sinking</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146918#M7420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks a lot Mac.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Oct 2009 08:27:23 GMT</pubDate>
    <dc:creator>layman</dc:creator>
    <dc:date>2009-10-16T08:27:23Z</dc:date>
    <item>
      <title>IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146911#M7413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am reading the datasheet of the MC9SH8QG4 and I see next data:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maximum total IOH for all port pins | IOHT | — 60 mA&lt;/P&gt;&lt;P&gt;Maximum total IOL for all port pins IOLT — 60 mA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to power about 8 leds, and each one has a current consumptiom about 50mA. Can I power the leds directly with the microcontroller or shall I need to use transistors? I am not sure if the "maximum total IOL/H" is for one pin or all the pins of the microcontroller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2009 15:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146911#M7413</guid>
      <dc:creator>PW_CTL</dc:creator>
      <dc:date>2009-10-14T15:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146912#M7414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;This is the sum of all the pins sinking or sourcing at any one time. You will need some form of external driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2009 18:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146912#M7414</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-10-14T18:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146913#M7415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks. Then, I´ll put some little transistors.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2009 18:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146913#M7415</guid>
      <dc:creator>PW_CTL</dc:creator>
      <dc:date>2009-10-14T18:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146914#M7416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a similar confusion with MC9S08SG8. I want to power a 10ma led directly with the controller. All other i/o pins are not sourcing/sinking any significant current. The datasheet does not seem to set any limit on individual pin but there is an overall limit of (Max total IOH for all ports OHT/OLT = –/+100 mA.Can any one please confirm that its safe to sink 10mA thru a single pin of MC9S08SG8 ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Pramod&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2009 11:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146914#M7416</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-15T11:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146915#M7417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pramod,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sinking 10 mA at a single pin is quite OK (this thread originally refered to sinking 50 mA). However, you will need a suitable series connected resistor to limit the LED current.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actually, for this current level to be reliably achieved, a Vdd of 5 volts will be necessary, in conjunction with high drive current.&amp;nbsp; Even so, the LED current may vary from unit-to-unit because the the pin output voltage may be up to 1.5 volts with this level of sink current (think of this as a variable output resistance up to 150 ohms maximum).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by bigmac on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-15&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;06:28 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2009 14:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146915#M7417</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-10-15T14:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146916#M7418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mac, Thanks for the detailed reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The orignal post was about MC9SH8QG4 while I am using MC9S08SG8.&lt;/P&gt;&lt;P&gt;Being a newbie to freescale, just wanted to be sure before I send the gerber out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the datasheet, I can see that for ILoad = 10 mA. Output low voltage (Max)= 0.8. I understand that this means that my pin voltage can be anything between 0 and 0.8 instead of&amp;nbsp; being exactly equal to 0.&lt;/P&gt;&lt;P&gt;Is this the phenomenon that you are refering to when you say "variable output resistance up to 150 ohms " ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am i correct in saying that the Variable o/p resistance can be anything between 0 at 80 ohm ?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pramod&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2009 16:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146916#M7418</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-15T16:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146917#M7419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pramod,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did actually check a copy of the datasheet for the 'SG8 device, and the specified maximum voltage was 1.5 volts at 10mA.&amp;nbsp; This was a preliminary version, so perhaps the specification has changed for the latest datasheet.&amp;nbsp; Based on the figure you quoted, the maximum output resistance would indeed be 80 ohms.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The minimum resistance would never be zero, but I guess might possibly reduce by a factor of two or three for some devices.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2009 02:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146917#M7419</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-10-16T02:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: IO current sinking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146918#M7420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks a lot Mac.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2009 08:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IO-current-sinking/m-p/146918#M7420</guid>
      <dc:creator>layman</dc:creator>
      <dc:date>2009-10-16T08:27:23Z</dc:date>
    </item>
  </channel>
</rss>