<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: 6LowPan  over mc1322x</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146419#M7322</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2011 20:36:06 GMT</pubDate>
    <dc:creator>sbeeem</dc:creator>
    <dc:date>2011-07-20T20:36:06Z</dc:date>
    <item>
      <title>6LowPan  over mc1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146416#M7319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use a 6lowpan protocol over the ieee 802.15.4.&lt;/P&gt;&lt;P&gt;With the dongle sniffer and WireShark i saw the packet "in the air" but the coordinator doesn't receive it correctly.&lt;/P&gt;&lt;P&gt;It receive the first part of the packet that is the header of 802.15.4 correctly but the 6lowpan header and the payload(sensor data)&amp;nbsp; are random value. Also after the first 5 packet the end device stop transmitting data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is simple, witch is the problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the packet is longer than the standard the coordinator's buffer is not enough?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is my code, we fill the packet with a function that return the pointer to the 6lowpan struct. I fill the fields with default value. But I think that the error is in the coordinator source code because the packet is correctly formed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;typedef struct pkt_6LowPan_t&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/*Header Ipv6*/&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;uint8_t&amp;nbsp;&amp;nbsp; dispatch;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Byte iniziale 6LP normalmente vale 01000001 per uncompressed ipv6*/&lt;BR /&gt;&amp;nbsp;uint8_t&amp;nbsp;&amp;nbsp; version_traffic_flow[4];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Version traffic e flow label*/&lt;BR /&gt;&amp;nbsp;uint8_t&amp;nbsp;&amp;nbsp; payload_len[2];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*lunghezza pacchetto*/&lt;BR /&gt;&amp;nbsp;uint8_t&amp;nbsp;&amp;nbsp; next_header;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*tipo header successivo*/&lt;BR /&gt;&amp;nbsp;uint8_t&amp;nbsp;&amp;nbsp; hop_limit;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*numero di hop massimi (serve nel routing)*/&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;/*Indirizzi*/&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;long int&amp;nbsp;&amp;nbsp; srcdestaddress[8];&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;/*Data*/&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;//uint8_t p6Msdu[8];&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;} pkt6LowPan_t;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*definizione del puntatore all'inizio del pacchetto, inizializzato a null*/&lt;BR /&gt;&lt;BR /&gt;/*--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------*/&lt;BR /&gt;//-----------------------------------------------------------------------------------&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;// Type: gMcpsDataInd_c,&lt;BR /&gt;typedef struct mcpsDataInd_tag {&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; dstAddr[8];&amp;nbsp;&amp;nbsp;&amp;nbsp; // First 0/2/8 bytes is the address as defined by dstAddrMode&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; dstPanId[2];&amp;nbsp;&amp;nbsp; // 16 bit word converted to little endian byte array&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; dstAddrMode;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; srcAddr[8];&amp;nbsp;&amp;nbsp;&amp;nbsp; // First 0/2/8 bytes is the address as defined by srcAddrMode&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; srcPanId[2];&amp;nbsp;&amp;nbsp; // 16 bit word converted to little endian byte array&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; srcAddrMode;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; msduLength;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 0-102 (101?)&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; mpduLinkQuality;&lt;BR /&gt;&amp;nbsp; bool_t&amp;nbsp;&amp;nbsp; securityUse;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; aclEntry;&lt;BR /&gt;&amp;nbsp; pkt6LowPan_t p6LowPan;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; *pMsdu;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Data will start at this address inside the message.&lt;BR /&gt;} mcpsDataInd_t;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks to all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2011 19:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146416#M7319</guid>
      <dc:creator>sbeeem</dc:creator>
      <dc:date>2011-07-04T19:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: 6LowPan  over mc1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146417#M7320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I saw that the end device stop sending Poll request to coordinator, and in Uart appear the message packet dropped, but I don't know why.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2011 20:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146417#M7320</guid>
      <dc:creator>sbeeem</dc:creator>
      <dc:date>2011-07-04T20:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: 6LowPan  over mc1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146418#M7321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should take a look at the mc1322x project:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mc1322x.devl.org" rel="nofollow" target="_self"&gt;http://mc1322x.devl.org&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We already have 6lowpan, RPL, and CoAP running on the mc13224v using Contiki.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Mar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Jul 2011 20:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146418#M7321</guid>
      <dc:creator>redbee</dc:creator>
      <dc:date>2011-07-10T20:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: 6LowPan  over mc1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146419#M7322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2011 20:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/6LowPan-over-mc1322x/m-p/146419#M7322</guid>
      <dc:creator>sbeeem</dc:creator>
      <dc:date>2011-07-20T20:36:06Z</dc:date>
    </item>
  </channel>
</rss>