<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Interfacing MC9S08GT60 SCI to a FTDI USB Adapter...</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-MC9S08GT60-SCI-to-a-FTDI-USB-Adapter/m-p/145898#M7269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Ed,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;If the FTDI device and the MCU are supplied from the same 3.3 volt&amp;nbsp;regulator, i.e. derived from the USB interface, the inclusion of series resistors won't be necessary.&amp;nbsp; However, if the two devices are supplied from separate regulators, and&amp;nbsp;using two different&amp;nbsp;power sources, I would tend to include series resistors, perhaps 2k2 or 4k7, to be sure.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Sep 2007 10:57:42 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2007-09-14T10:57:42Z</dc:date>
    <item>
      <title>Interfacing MC9S08GT60 SCI to a FTDI USB Adapter...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-MC9S08GT60-SCI-to-a-FTDI-USB-Adapter/m-p/145897#M7268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Guys,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm getting a bit confused about the voltage compatibilities when interfacing the GT60 MCU to an FTDI SERIAL-USB transceiver... That's because I don't understand what exactly TTL and CMOS mean.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The voltage levels of the MCU IO ports, according to the datasheet, are (VDD = 3.3V):&lt;/DIV&gt;&lt;DIV&gt;Vout Hi&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VDD - 0.5 ( so =2.8V)&lt;/DIV&gt;&lt;DIV&gt;Vout Low&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;0.5V&lt;/DIV&gt;&lt;DIV&gt;Vin&amp;nbsp; Low&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.35 x VDD ( so = 1.15)&lt;/DIV&gt;&lt;DIV&gt;Vin&amp;nbsp; Hi&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.7 x VDD&amp;nbsp; (so = 2.31)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The FTDI "cable" I am intending to use is on&lt;/DIV&gt;&lt;DIV&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.ftdichip.com%2FProducts%2FEvaluationKits%2FTTL-232R-3V3-PCB.htm" rel="nofollow" target="_blank"&gt;http://www.ftdichip.com/Products/EvaluationKits/TTL-232R-3V3-PCB.htm&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I read the app note AN2433 but&amp;nbsp;I'm still confused...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;And the confusion is that acording to the App Note,&amp;nbsp;I will need to&amp;nbsp;use a resistor between the &amp;nbsp;MCU SCI and the TTL port of the FTDI device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;However, the FTDI Datasheet (in attach) says that the input threshold is&amp;nbsp;1.2V and the output voltage levels are&amp;nbsp;2.8V (Hi) and 0.4V (Low)...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So, can I just plug it in without burning something?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The other FTDI chip I've been using (FT232BM) works just fine with no resistors, as there is a pin VCC_IO that is supplied with 3.3V and it limits the&amp;nbsp;IO voltage values to 1.2V, 2.7 and 0.4.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;As the Voltage levels are the same for the old chip&amp;nbsp;and this new cable I want to use, Is there anything&amp;nbsp;else that I need to be aware ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Just to make sure.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers mates,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Ed.&lt;/DIV&gt;&lt;DIV&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Ffiles%2Fcommunity_files%2F8BITCOMM%2F7449_DS_TTL232R3V3.pdf" rel="nofollow" target="_blank"&gt;DS_TTL232R3V3.pdf&lt;/A&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;01:22 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2007 06:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-MC9S08GT60-SCI-to-a-FTDI-USB-Adapter/m-p/145897#M7268</guid>
      <dc:creator>ehestigoni</dc:creator>
      <dc:date>2007-09-14T06:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing MC9S08GT60 SCI to a FTDI USB Adapter...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-MC9S08GT60-SCI-to-a-FTDI-USB-Adapter/m-p/145898#M7269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Ed,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;If the FTDI device and the MCU are supplied from the same 3.3 volt&amp;nbsp;regulator, i.e. derived from the USB interface, the inclusion of series resistors won't be necessary.&amp;nbsp; However, if the two devices are supplied from separate regulators, and&amp;nbsp;using two different&amp;nbsp;power sources, I would tend to include series resistors, perhaps 2k2 or 4k7, to be sure.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2007 10:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-MC9S08GT60-SCI-to-a-FTDI-USB-Adapter/m-p/145898#M7269</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-09-14T10:57:42Z</dc:date>
    </item>
  </channel>
</rss>