<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: What's capacitor for oscillator? MC9S08LC36</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145476#M7185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I don't think this is related to the oscillator, and the cap values aren't all that critical. 18pF should work fine.&lt;BR /&gt;&lt;BR /&gt;Instead I strongly suspect the low-voltage detection is reseting the circuit, as it should. This kicks at around 2.6V. Have you configured the LVD properly for lower voltages?&lt;BR /&gt;&lt;BR /&gt;You should be able to easily determine if this is the problem or not, by checking the reset pin of the MCU with an oscilloscope.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2009 18:43:50 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2009-01-23T18:43:50Z</dc:date>
    <item>
      <title>What's capacitor for oscillator? MC9S08LC36</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145475#M7184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi,&lt;BR /&gt;I use MC9S08LC36 with oscillator at 2MHz.&lt;BR /&gt;I must use the&amp;nbsp; micro at 3V but my Vcc can be less 3V (example 2.6V).&lt;BR /&gt;At 2.8V the oscillator don't run!&lt;BR /&gt;I suppose wrong capacitor (I have try 10pF and 18pF).&lt;BR /&gt;I have try to change ICGTRM but don't run!&lt;BR /&gt;&lt;BR /&gt;It run only at 3V.&lt;BR /&gt;What's capacity I must insert with 2Mhz of oscillator?&lt;BR /&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Added p/n to subject.&lt;BR /&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2009-01-22&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;08:55 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2009 17:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145475#M7184</guid>
      <dc:creator>cicciounico</dc:creator>
      <dc:date>2009-01-22T17:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: What's capacitor for oscillator? MC9S08LC36</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145476#M7185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I don't think this is related to the oscillator, and the cap values aren't all that critical. 18pF should work fine.&lt;BR /&gt;&lt;BR /&gt;Instead I strongly suspect the low-voltage detection is reseting the circuit, as it should. This kicks at around 2.6V. Have you configured the LVD properly for lower voltages?&lt;BR /&gt;&lt;BR /&gt;You should be able to easily determine if this is the problem or not, by checking the reset pin of the MCU with an oscilloscope.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2009 18:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145476#M7185</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2009-01-23T18:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: What's capacitor for oscillator? MC9S08LC36</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145477#M7186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks!&lt;BR /&gt;The LVD is disable.&lt;BR /&gt;The reset is alwais high.&lt;BR /&gt;I have test my board with Vcc=2.8V and I have see XTAL (PTB1) alwais high. If I tap the pin of microcontroller with a finger the oscillator wakeup and it run then I suppose is the oscillator.&lt;BR /&gt;My supposition is wrong?&lt;BR /&gt;Vcc is not to low, is 2.8V.&lt;BR /&gt;Thanks again!&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jan 2009 21:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145477#M7186</guid>
      <dc:creator>cicciounico</dc:creator>
      <dc:date>2009-01-26T21:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: What's capacitor for oscillator? MC9S08LC36</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145478#M7187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Now work!&lt;BR /&gt;I have change oscillator from 2MHz to 32KHz.&lt;BR /&gt;Now at 2.4V work fine and the oscillator run it.&lt;BR /&gt;&lt;BR /&gt;thanks.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2009 01:05:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/What-s-capacitor-for-oscillator-MC9S08LC36/m-p/145478#M7187</guid>
      <dc:creator>cicciounico</dc:creator>
      <dc:date>2009-01-27T01:05:03Z</dc:date>
    </item>
  </channel>
</rss>