<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 RTI is not working in Run/Wait mode (on Stop 3 does work) in 9S08GT32!</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RTI-is-not-working-in-Run-Wait-mode-on-Stop-3-does-work-in/m-p/125692#M715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;SPAN style="font-size: 2;"&gt;I am working with 9S08GT32 controller where part of the time my code goes into Stop 3 mode and part of the time the code is in RUN, Wait mode. I am using internal 1kHz clock generator for RTI interrupts. Normally in Run/Wait modes I am working in FEI ICG mode with Bus Clock of 15.552MHz and upon entrance to Stop3 mode, I am going to SCM ICG mode, lowering clock frequency. After receiving an RTI interrupt and terminating Stop 3 mode, the code is returning back to FEI mode. The RTI interrupt routine clears the RTIF flag (by RTIACK), and the SPMSC2_PPDF flag (by SPMSC2_PPDACK). Anyway after exit from Stop3 the RTI interrupts do stop. (In running mode or wait mode) and resume only upon entrance back to Stop 3 mode. What could be a reason for this phenomenon that RTI is not interrupting in the Run/Wait mode? Additional input is that while in BDM mode (background debug mode) the RTI interrupts do not arrive too. I have to simulate their arrival, through the debugging session.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Feb 2006 19:26:44 GMT</pubDate>
    <dc:creator>yasha11</dc:creator>
    <dc:date>2006-02-01T19:26:44Z</dc:date>
    <item>
      <title>RTI is not working in Run/Wait mode (on Stop 3 does work) in 9S08GT32!</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RTI-is-not-working-in-Run-Wait-mode-on-Stop-3-does-work-in/m-p/125692#M715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;SPAN style="font-size: 2;"&gt;I am working with 9S08GT32 controller where part of the time my code goes into Stop 3 mode and part of the time the code is in RUN, Wait mode. I am using internal 1kHz clock generator for RTI interrupts. Normally in Run/Wait modes I am working in FEI ICG mode with Bus Clock of 15.552MHz and upon entrance to Stop3 mode, I am going to SCM ICG mode, lowering clock frequency. After receiving an RTI interrupt and terminating Stop 3 mode, the code is returning back to FEI mode. The RTI interrupt routine clears the RTIF flag (by RTIACK), and the SPMSC2_PPDF flag (by SPMSC2_PPDACK). Anyway after exit from Stop3 the RTI interrupts do stop. (In running mode or wait mode) and resume only upon entrance back to Stop 3 mode. What could be a reason for this phenomenon that RTI is not interrupting in the Run/Wait mode? Additional input is that while in BDM mode (background debug mode) the RTI interrupts do not arrive too. I have to simulate their arrival, through the debugging session.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2006 19:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RTI-is-not-working-in-Run-Wait-mode-on-Stop-3-does-work-in/m-p/125692#M715</guid>
      <dc:creator>yasha11</dc:creator>
      <dc:date>2006-02-01T19:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: RTI is not working in Run/Wait mode (on Stop 3 does work) in 9S08GT32!</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RTI-is-not-working-in-Run-Wait-mode-on-Stop-3-does-work-in/m-p/125693#M716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I have the same pb in BDM mode, the RTI ISR doesn't arrive.&lt;/DIV&gt;&lt;DIV&gt;But without the BDM cable, it's ok.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yvan&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2006 21:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RTI-is-not-working-in-Run-Wait-mode-on-Stop-3-does-work-in/m-p/125693#M716</guid>
      <dc:creator>yb</dc:creator>
      <dc:date>2006-02-01T21:19:16Z</dc:date>
    </item>
  </channel>
</rss>