<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Clock Sources on MC1321x</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145281#M7122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Strikecity,&lt;BR /&gt;&lt;BR /&gt;if you see at paragraph 3.5 look at Figure 3-3. MC1321x Clock Connections,&lt;BR /&gt;I don't understand if it's possible to connect both clock sources.&lt;BR /&gt;Probably if both clock sources are connected you can't make the connection&lt;BR /&gt;between pin 9 and 10, but the S08 section has 32kHz source and radio has his 16MHz&lt;BR /&gt;clock source.&lt;BR /&gt;&lt;BR /&gt;Doubts about the synchronization between radio and S08.....&lt;BR /&gt;&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2007 17:38:43 GMT</pubDate>
    <dc:creator>stevasway</dc:creator>
    <dc:date>2007-02-16T17:38:43Z</dc:date>
    <item>
      <title>Clock Sources on MC1321x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145279#M7120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Is it possible to connect both clock source on MC1321x&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in order to use 16MHz when radio modem is on, and 32kHz when&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I switch off the radio and run only the S08 micro section?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To obtain ultra low power, I need to switch on the radio modem&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;only when I need, but I need a S08 section running without&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;using internal (not exact) clock sources.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Stevasway&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2007 21:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145279#M7120</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2007-02-15T21:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: Clock Sources on MC1321x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145280#M7121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;stevesaway,&lt;BR /&gt;&lt;BR /&gt;I'm looking at pages 7 and 9 of the MC1321x datasheet... it looks like the 16MHz radio crystal only drives the S08 core if pins 9 and 10 are connected. If you don't make this connection, you can drive the core at any frequency.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2007 22:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145280#M7121</guid>
      <dc:creator>strikecity</dc:creator>
      <dc:date>2007-02-15T22:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: Clock Sources on MC1321x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145281#M7122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Strikecity,&lt;BR /&gt;&lt;BR /&gt;if you see at paragraph 3.5 look at Figure 3-3. MC1321x Clock Connections,&lt;BR /&gt;I don't understand if it's possible to connect both clock sources.&lt;BR /&gt;Probably if both clock sources are connected you can't make the connection&lt;BR /&gt;between pin 9 and 10, but the S08 section has 32kHz source and radio has his 16MHz&lt;BR /&gt;clock source.&lt;BR /&gt;&lt;BR /&gt;Doubts about the synchronization between radio and S08.....&lt;BR /&gt;&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2007 17:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Clock-Sources-on-MC1321x/m-p/145281#M7122</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2007-02-16T17:38:43Z</dc:date>
    </item>
  </channel>
</rss>