<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Who-Tell-me-the-different-between-MC908QL4MDW1-and-MC908QL4MDW2/m-p/143882#M6706</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Harlan -&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There was a problem with a mask set that the internal clock would not trim to the 25.6 MHz option. These parts are marked with the '1'.&amp;nbsp; Parts that will trim correctly at 25.6 MHz are marked with '2'.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you are using an external crystal or if you are using the internal at 4, 8, or 12.8 MHz, then this won't make a difference.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;- Rocky&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2007 22:51:27 GMT</pubDate>
    <dc:creator>RockyRoad</dc:creator>
    <dc:date>2007-01-30T22:51:27Z</dc:date>
    <item>
      <title>Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Who-Tell-me-the-different-between-MC908QL4MDW1-and-MC908QL4MDW2/m-p/143881#M6705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;We use the MC908QL4MDW.. But the logo on IC is MC908QL4MDW1? And sometimes, the logo is MC908QL4MDW2?&amp;nbsp; I want to konw the different??? I can not get the information about the '1' or '2' from the datasheet.&lt;/DIV&gt;&lt;DIV&gt;thx&lt;/DIV&gt;&lt;DIV&gt;Harlen&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2007 10:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Who-Tell-me-the-different-between-MC908QL4MDW1-and-MC908QL4MDW2/m-p/143881#M6705</guid>
      <dc:creator>harlenChen</dc:creator>
      <dc:date>2007-01-30T10:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Who-Tell-me-the-different-between-MC908QL4MDW1-and-MC908QL4MDW2/m-p/143882#M6706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Harlan -&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There was a problem with a mask set that the internal clock would not trim to the 25.6 MHz option. These parts are marked with the '1'.&amp;nbsp; Parts that will trim correctly at 25.6 MHz are marked with '2'.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you are using an external crystal or if you are using the internal at 4, 8, or 12.8 MHz, then this won't make a difference.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;- Rocky&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2007 22:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Who-Tell-me-the-different-between-MC908QL4MDW1-and-MC908QL4MDW2/m-p/143882#M6706</guid>
      <dc:creator>RockyRoad</dc:creator>
      <dc:date>2007-01-30T22:51:27Z</dc:date>
    </item>
  </channel>
</rss>