<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08QG8: 32.768Khz External Xtal or RTC - Current consumption?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143735#M6684</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;A small tip as you are new to Freescale MCUs.&lt;BR /&gt;Freescale specifications are re-known to be extremely worst case.&lt;BR /&gt;Your device will much more probably be closer to the typical than the maximum.&lt;BR /&gt;&lt;BR /&gt;It will depend a lot on the temperature profile of the application.&lt;BR /&gt;&lt;BR /&gt;Jojo.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 28 Jan 2007 01:24:18 GMT</pubDate>
    <dc:creator>Nabla69</dc:creator>
    <dc:date>2007-01-28T01:24:18Z</dc:date>
    <item>
      <title>MC9S08QG8: 32.768Khz External Xtal or RTC - Current consumption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143733#M6682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;I am new to Freescal MCUs, what I know is just from reading the app notes and DSs.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Coming from the msp430 with extremely low current consumption with an active RTC&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;during "sleep" (msp430 LPM3 ~ Freescale stopx) I have been trying to understand if&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;the same low current consumption (msp430F20XX: 500nA)&amp;nbsp; is &amp;nbsp;possible with Freescale MCUs.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;(I am not trying to promote the msp430 here, in fact I am considering a defection), so this&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;thread was of great interest to me.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;However, the reason I am jumping in is the mentioning in the previous postings&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;of the need for an external RTC IC.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;There is probably something I have missed here. It seems to&amp;nbsp;me this is&amp;nbsp;possible with just&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;an external 32,768 kHz crystal on the MC9S08QG8 (16 pin version) EXTAL/XTAL pins?&lt;/DIV&gt;&lt;DIV&gt;The DS "&lt;STRONG&gt;MC9S08QG8 and MC9S08QG4 Data Sheet, Rev. 1.01" (page 264)&lt;/STRONG&gt;.&lt;/DIV&gt;&lt;DIV&gt;Current consumption during stop3 would then be around 6uA (3v).&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;10x the msp430F20XX, but still&amp;nbsp;so low that a&amp;nbsp;coin cell&amp;nbsp;battery,&amp;nbsp;say CR2032, &amp;nbsp;would last 4-5 years,&lt;/DIV&gt;&lt;DIV&gt;which is acceptable&amp;nbsp;(not great) for my application.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope somebody in-the-know in this news group could clarify this, e.g. for deep low current consumption, do&lt;/DIV&gt;&lt;DIV&gt;you need an external RTC IC or will a locally connected watch crystal do (if you can accept 6uA during stop3)?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank You&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Peter K&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: 1;"&gt;(Alban split to new post: new question = new post&amp;nbsp;to ease&amp;nbsp;clarity and search)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-01-27&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;05:09 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jan 2007 00:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143733#M6682</guid>
      <dc:creator>PeterK</dc:creator>
      <dc:date>2007-01-28T00:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8: 32.768Khz External Xtal or RTC - Current consumption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143734#M6683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Peter,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You don't need an external RTC.&lt;/DIV&gt;&lt;DIV&gt;The QG8 contains an AWU or PWU = Auto/Periodic Wake-Up module.&lt;/DIV&gt;&lt;DIV&gt;This is using an RC oscillator with low power consumption.&lt;/DIV&gt;&lt;DIV&gt;The software can correct any lack of precision this clock might have if this is critical.&lt;/DIV&gt;&lt;DIV&gt;A crystal will be sufficient (and much cheaper)&amp;nbsp;and will not be powered when in very low consumption mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The consumption of the QG8 is lower than 6uA. The measure is a &lt;STRONG&gt;max&lt;/STRONG&gt; @ &lt;STRONG&gt;85C&lt;/STRONG&gt;.&lt;/DIV&gt;&lt;DIV&gt;If you look, the typical value is 750nA.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To lower consumption, you can also play with clock speeds. Not to use full speed when not required will lower the overall consumption.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jan 2007 01:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143734#M6683</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-28T01:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8: 32.768Khz External Xtal or RTC - Current consumption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143735#M6684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;A small tip as you are new to Freescale MCUs.&lt;BR /&gt;Freescale specifications are re-known to be extremely worst case.&lt;BR /&gt;Your device will much more probably be closer to the typical than the maximum.&lt;BR /&gt;&lt;BR /&gt;It will depend a lot on the temperature profile of the application.&lt;BR /&gt;&lt;BR /&gt;Jojo.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jan 2007 01:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-32-768Khz-External-Xtal-or-RTC-Current-consumption/m-p/143735#M6684</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2007-01-28T01:24:18Z</dc:date>
    </item>
  </channel>
</rss>