<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 LIN bus -wake up needed for test</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LIN-bus-wake-up-needed-for-test/m-p/143427#M6598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm desperate to solve a LIN-bus sensor problem. I connected two angle sensors from a car to a power source and a oscilloscope to the output pin of the sensor. I guess one sensor is the master and the other is a slave. But there is nothing coming out from the sensors. I was expecting a PWM-signal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My qeustion, is the sensors expecting a wake-up signal before they will deliver any kind of data stream. Do I need a lin-bus simulator to send the wake-up and determine if the sensor is broken?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I really try to achieve is a out of the car test bench so I can set up a LIN-bus device and determine if it is broken.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll be thankfull for any advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Aug 2007 13:22:31 GMT</pubDate>
    <dc:creator>jaras</dc:creator>
    <dc:date>2007-08-21T13:22:31Z</dc:date>
    <item>
      <title>LIN bus -wake up needed for test</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LIN-bus-wake-up-needed-for-test/m-p/143427#M6598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm desperate to solve a LIN-bus sensor problem. I connected two angle sensors from a car to a power source and a oscilloscope to the output pin of the sensor. I guess one sensor is the master and the other is a slave. But there is nothing coming out from the sensors. I was expecting a PWM-signal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My qeustion, is the sensors expecting a wake-up signal before they will deliver any kind of data stream. Do I need a lin-bus simulator to send the wake-up and determine if the sensor is broken?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I really try to achieve is a out of the car test bench so I can set up a LIN-bus device and determine if it is broken.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll be thankfull for any advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2007 13:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LIN-bus-wake-up-needed-for-test/m-p/143427#M6598</guid>
      <dc:creator>jaras</dc:creator>
      <dc:date>2007-08-21T13:22:31Z</dc:date>
    </item>
    <item>
      <title>Re: LIN bus -wake up needed for test</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LIN-bus-wake-up-needed-for-test/m-p/143428#M6599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Your information seems to be confusing. First, LIN does not work w/ pwm signals on LIN data line. Maybe it could be SAE J1850.&amp;nbsp; Second, it is strange to me hear that one sensor is a master and another is a slave. Normally the master is an ECU connected to a CAN network.&lt;BR /&gt;&lt;BR /&gt;Before desperate attempts, try to get more info on your particular system.&lt;BR /&gt;&lt;BR /&gt;If it is really LIN and if you just really need a wake up, it is quite easy, just drop the LIN line low for at least 150us.&lt;BR /&gt;&lt;BR /&gt;I hope it helps.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;&lt;BR /&gt;Celso&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2007 19:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LIN-bus-wake-up-needed-for-test/m-p/143428#M6599</guid>
      <dc:creator>celsoken</dc:creator>
      <dc:date>2007-08-21T19:51:43Z</dc:date>
    </item>
  </channel>
</rss>